Part Number: ISO7761-Q1 Other Parts Discussed in Thread: ISO7761 , , SN74LVC125A Tool/software: Hello, I designed an SPI circuit using ISO7761 BUFFER as shown in the attached picture.
There are 5 SLAVEs connected to one SPI line. Are there any problems…
Part Number: ISO7761-Q1 Hi Expert,
My customer is facing shortage on ISO7761FQDBQRQ1. May you kindly check if we have P2P replacement for this device? No need to change the schematic/layout.
Thanks!
Ethan Wen
Part Number: ISO7761-Q1
Hello,
We are using ISO7761FQDWQ1 digital isolator in our design.
I want to confirm below point:
In the ISO7761FQDWQ1 IC, 5 channel are forward and 1 is reverse, Considering this case:
Vcci/Vcc1 is the input power supply…
Hello,
Thank you for your question.
The FIT rate described in ISO7761-Q1 Functional Safety, FIT Rate, Failure Mode Distribution and Pin FMA document is functional safety FIT. This is used in a functional safety application for safety analysis.
All…
Part Number: ISO6741-Q1 Other Parts Discussed in Thread: ISO6760-Q1 , ISO7741-Q1 , ISO7760-Q1 , ISO7761-Q1 , ISO6761-Q1 Hi Im looking for alternate part for ISO6741-Q1 with 5/0, 5/1 , 6/0 or more channels Isolator. I need enable control on output. Please…
Part Number: ISO7761 I am using ISO7761. The data sheet states the following, but I think the actual operation is different from the description. Attached is the circuit diagram and waveforms.
According to the data sheet, when VCCI is PD (<1.7V) and…
Part Number: ISO6762 Hello,
we were wondering, why the ISO6762 is neither listed in the UL File No. FPPT8.E181974, nor in the UL-CA-L181974-24-32205102-8, even though it is mentioned under "PRODUCTs COVERED" in "USR/CNR - Single Protection, Non-Optical…