Part Number: ISO7820LL Tool/software: Hi Sir,
May I know have any isolated LVDS buffer device with data rate up to 1.1Gbps? I would like use it to replace the ADI / ADN4654BRWZ-RL7?
Part Number: ISO7820LL
Hi,
We are using TI isolator to interface the differential clock signals from FPGA to the ADC as shown in the image.
We have the following two concerns.
1) Please let us know if the LVDS Signal specs mentioned in the image…
Part Number: ISO7820LL Other Parts Discussed in Thread: ISO7821LLS Hi team,
Could you please kindly help check if we have device to replace ADI's ADN4654BRWZ-RL7?
Thanks,
Brian
Part Number: ISO7820LL Other Parts Discussed in Thread: ISO1640 , ISO7730 , ISO7760 Hello,
design it to insulate between the graphic processor and TFT LCD as follows.
There are various Isolation ICs in the power, but I cannot find Isolation ICs…
Part Number: ISO7820LL Hi team,
My customer is considering to use ISO7820LL and have a question about the tsk(pp).
In the datasheet, maximum value for tsk(pp) is 4.5ns.
If there is device A and B, there will be a worst cases that A is lagged ±4…
Part Number: ISO7820LL Hit team,
For ISO7820LL, datasheet says tsk of this device is
tsk(o) Max2.5ns
tsk(pp) Max4.5ns
Does this means that the maximum skew time for the 4 channels is tsk(pp)+tsk(o)=4.5ns+2.5ns=7.0ns?
Regards,
Ohashi
Part Number: ISO7820LL The http://www.ti.com/quality/docs/estimator.tsp does currently not provide any data about the Digital Isolators. I notice that behavior already in the past and sometime later (few month) the data were available again. Is there…
Part Number: ISO7820LL Having the inputs and outputs P M M P makes it very inconvenient to connect. Is it possible to connect as P M P M on both sides and have the signals function properly?
Best regards,
Stuart Borden.
Part Number: ISO7820LL Hi,
I use ISO7820LL to transmit LVDS signal. But i met a question on GND.
Please refer below schematic,
If 3(the VCC1 GND of ISO7820LL) is connection for VCC1, OUTA+ and OUTA-(FP_SYNC_P, FP_SYNC_N) is no output.
If 3(the…