Part Number: ISO7842 Other Parts Discussed in Thread: ISO7840 Tool/software: Hello,
according to the datasheet, the maximum allowed value of the output current of ISO7842 is 15 mA. Is it allowed to connect an RC circuit consisting of serially connected…
Part Number: ISO7820 Other Parts Discussed in Thread: ISO7840 , ISO7842 Tool/software: Dear,
We use ISO7820 and ISO7840,UL 61010-1 2018 standard contains the definition of 5s - as follows, the current value of 5700VRMS 1min is OK, we do need the AC value…
Part Number: ISOW7840 Other Parts Discussed in Thread: ISO7840 , Tool/software: Hi Expert,
This is Shenzhen FAE Evan. My customer is evaluating ISO7840, in their scenario, in integrated DCDC should transfer 3.3V to 5V. And they will also connect about…
Part Number: ISO7840
Hi all Just in case, we would like to confirm ISO7840F's function table.
<ISO7840F's function table which we assume> Vcci : PU, Vcco : PU, INX : High , EN2 : High or Open -> OUTX : Low Vcci : PU, Vcco : PU, INX : Low…
Part Number: ISO7840 Hi all Would you mind if we ask ISO7840? Input voltage of Absolute Maximum Ratings is VCCX + 0.5V. If voltage applies to INX without VCC1 supply(no power supply), it exeeds Absolute Maximum Ratings. Does it means there is internal protection…
Part Number: ISO7840 Hi all Would you mind if we ask ISO7840? <Question1> How much is the capacitance value at each pins? If you have these data, could you give us as the reference? <Question2> On the datasheet Figure.17 P20, we guess that "Input (Device…
Hello,
Thank you for your inquiry.
We do not have a wider package for the ISO7240C device.
However, we do have other digital isolator devices with a larger package size, such as the ISO7840 device. The ISO7840 is available in a larger ultra-wide body…
Hi all, Would you mind if we ask ISO784X(reiforced degital isolator) series? <Question1> About Reinforced isolation, the minimum creepage distance which based on IEC60950 is 6.4mm. In case of ISO784X, we think the shortest distance along the surface of the…
Part Number: ISOW7840 Other Parts Discussed in Thread: ISO7840 , ISO7740 , ISO6740 , ISO7741 Hi,
I would like to use the isow7840 digital isolator to drive with an FPGA, the synchronization lines of four hydrophones submerged in water. The hydrophones are…
Part Number: ADS127L01 Other Parts Discussed in Thread: ISO7740 , ISO7840 Hello Team,
My customer is looking for the best-fit SPI digital Isolator for ADS127L01. Can you suggest one?
Regards,
Renan