Part Number: ISOUSB111 Hi ,
I am currently evaluating the ISOUSB111 for use in an upcoming new project.
However, I have been monitoring the inventory on the TI website for the past month, and the stock has consistently remained at zero with no…
Part Number: ISOUSB111 Hi,
we are designing a isolated USB 2.0 FS industrial peripheral with USB C connector.
The MCU USB internal USB module is configured as Peripheral.
The DD side of the isolator is supplied by the internal MCU supply.
The…
Part Number: ISOUSB111 e2e,
I’m looking for an alternative to the ADuM3160 USB digital isolator, and identified the ISOUSB111 as the closest match.
I have a question regarding the operating voltages for VBUS1 and VBUS2 on the ISOUSB111. The datasheet…
Part Number: ISOUSB111 Other Parts Discussed in Thread: ISOUSB211 Hello, I’m evaluating ISOUSB111 for USB 2.0 isolation in a system where both the host and the device are High-Speed capable.
I understand that ISOUSB111 supports only Low-Speed and Full…
Part Number: ISOUSB111 We have two new designs that are virtually identical other than different mechanical layouts. We have had a lot of problems in an industrial environment with electrical noise messing up in a big way USB communications to our controller…
Part Number: ISOUSB111 Hello,
I would like to know if the certification process for the SSOP package is now fully complete and if not, which certificates are missing compaired to the SOIC package.
I have seen the post about the DIN EN IEC 60747-17…
Part Number: ISOUSB111 Tool/software: Hello. When I changed ADuM3160 to ISOUSB111, it started working strangely. Please tell me how to solve this problem.
UD+/UD- are connected to USB microB and DD+/DD- are connected to the MCU's USB D+/D-. The USB…
Part Number: ISOUSB111
Hi team,
We observed transient overshoot/undershoot on the UD+ and UD− pins.
Observed minimum voltages:
UD− = -0.797 V
UD+ = -0.585 V
At the same time:
DD− = -0.391 V
DD+ = 0.016 V
The negative excursions…
Part Number: ISOUSB111DWXEVM Hello.
I am using a ISOUSB111DWX to isolate a full speed usb signal to an STM32F446.
I am observing some very werid behavior where to communication can be established correctly on windows hosts and NOT on mac hosts.
…
Part Number: ISOUSB111 Tool/software: Dear Specialists,
My customer is considering TUSB111 for explosion proof equipment and has a question.
I would be grateful if you could advise.
---
I have questions about ISOUSB111.
① Is this device a non…