Part Number: ISOW3080 Good Morning,
for the respin of our industrial product, I would like to use your new ISOW3080 product.
Could you let me know when it will be available for purchase?
Because I will produce the first prototype at the end of September…
Part Number: ISOW3080 Other Parts Discussed in Thread: ISOW3086 Dear,
Can I use the ISOW3080 in a new design? I saw that it is currently available only in pre-production status as XISOW3080.
I have the same question regarding the ISOW3086, which is…
Part Number: ISOW1412 Other Parts Discussed in Thread: ISOW3080
Hello, we are currently developing a product that uses the ISOW1412. We ran into EMC issues with it and are revising our layout. At the moment there is no stock of the ISOW1412 available…
Part Number: ISOW3086 Other Parts Discussed in Thread: ISOW1432 , ISOW1412 , , ISOW3080 We were using in one of our designs the ISOW1412, ISOW1432 which is now unavailable or out of stock everywhere we are looking at
As we are now redesigning the board…
Part Number: ISOW3080 Hi team,
Quick clarification question from the prelim datasheet:
Table 8.2 calls out a Hi-Z state until VDD is present, which makes sense, but we have an invalid operational state when VDDL is not present.
Is there any more…
Part Number: ISOW3080 I need to verify if ISOW3080DWE is P2P direct replacement with NOVOSENSE NSIP93086-DSWR.
Speed is not a problem: in my application we are using 38400bps
If No, please let me know the direct TI replacement.
Thanks in advance…
Part Number: ISOW3080 Other Parts Discussed in Thread: PROFIBUS , , THVD2450 Hi team,
I have two questions.
There are two option depending VISOOUT (5V or 3.3V). Customer want half-duplex RS485 Transceiver (no PROFINET), are both able to be used…
Part Number: ISOW1050 Other Parts Discussed in Thread: LM5169 , ISOW3080 , We require small numbers of the ISOW3080 and ISOW1050 and the buck converter LM5169 for our new BMS design. Since there is no stock to order these parts, like to get few samples…
Part Number: ISOW1412 Other Parts Discussed in Thread: ISOW3080 We are using two ISOW1412 devices placed directly next to each other on the same PCB, operating as an RS-485 repeater.
During EN 55032 Class B radiated emission testing, the design exceeds…
Hello E2E,
Following are the latest Isolation Solution from TI which can be used for Isolated RS485 applications:
Digital Isolator:
ISO6441 - ISO6441 data sheet, product information and support | TI.com
ISO6041 - ISO6041 data sheet, product…