Dawson Huang said:
Part Number: MMWAVEICBOOST
Hello,
we are a university team in Taiwan , and this is our problem:
Our IWR6843ISK-ODS board can't succeed to connect to computer .
We have done many tests even asked on E2E forum ,but none of those…
Hello,
Which board you are using for the measurement? Is it IWR6843ISK or IWR6843ISK-ODS board?
For the 2nd case, could you please try to avoid 62.1 GHz frequency and use other frequency band and see if this goes away?
For the 1st case also…
Hi Mayue,
Maximum Distance: The maximum gesture detection range for the above demo is up to 40cm as mentioned in the Test Results section.
Field of View:
The IWR6843ISK-ODS has a maximum 120° azimuth and 120° elevation FoV as mentioned on the…
Hi Shravan,
Please find the answers below:
May i know how these two different software versions of the out of box SDK influence the output of the sensor:
Both variants of the OOB demo processing chain provide the same output format which is described…
Part Number: AWR1642BOOST Other Parts Discussed in Thread: DCA1000EVM Hi, TI team,
I want to know that is it possible to export the intermediate data, sort of RangeFFT from Radar cube, DopplerFFT data from Radar cube or detect-matrix through LVDS? Just…
Hi Abdellah,
Abdellah Bouchama said: To have a point cloud representation of moving person in covered area, can i use the 6843EVM Alone (without the MMWAVEICBOOST board carrier)?
Yes. The Out of Box Demo and most other demos in the toolbox including…
Part Number: DCA1000EVM Other Parts Discussed in Thread: IWR6843ISK-ODS Hi,
I try to capture the raw data from the DCA1000EVM by using the DCA1000EVM CLI application.
The precompiled version in mmwave_studio_02_01_01_00\mmWaveStudio\PostProc on Windows…
I am trying the two different approach that TIREX suggest either Uniflash or CCS, but some of the demos does are not present in CCS and Uniflash give an error trying to open the COM port. I have alll three modules Standard, Overhead and AoP, but could…
Part Number: DCA1000EVM Other Parts Discussed in Thread: IWR6843ISK-ODS , IWR6843 Hello,
I'm trying to use DCA1000 with IWR6843ISK-ODS board to do some raw data captures.
I just installed mmWaveStudio and all the dependencies. I had set up the jumpers…
Part Number: IWR6843ISK-ODS Hi,
I am studying gtrack library of people count demo in the package below.
"C:\ti\mmwave_industrial_toolbox_3_4_0__win\mmwave_industrial_toolbox_3_4_0\labs\lab0020_pplcount_Overhead\src\common\gtrack"
I exported…