Part Number: J721EXCPXEVM Tool/software: Hello experts,
I am currently exploring the IPC functionality on the J721E. My goal is to enable communication between a process running on Linux and an RTOS application running on the R5 core.
I have tried…
Part Number: J721EXCPXEVM Other Parts Discussed in Thread: TDA4VM Tool/software: Hi TDA4VM Team.
Can you please check if J721 CP Board would be able to support USB-C with Dispplay function?
A customer asks if it is possible to design a display to…
Part Number: J721EXCPXEVM Other Parts Discussed in Thread: IWRL6432BOOST Tool/software: Hello TI expert,
My name is Ronnel. I am currently working with the IWRL6432BOOST (EVM) radar and would like to capture raw data via SPI-Protocol. A key requirement…
Part Number: J721EXCPXEVM Tool/software: I am trying to import the SDL module into our project. I've added the module as is, and I've created a CMake file. I am trying to compile it with the arm-none-eabi-gcc compiler. However, GCC cannot compile .asm…
Part Number: J721EXCPXEVM Tool/software: Hi Ti
When I was bring up the module s5k3b6s+max96717+ max9296, the iic communication was normal and the image receiver was normal. I confirmed that the setting was written normally, but the soc did not receive…
Part Number: J721EXCPXEVM Tool/software: Hi,
i found the address of 0xC2000000 for the scratch pad memory of the processor , but cant figure out on the memory map, which physical location this is .
please shed some light on that
regards, …
Part Number: J721EXCPXEVM Tool/software: Hi all,
We are using the J721EXCPXEVM with the J7200XSOMXEVM for our proyect development.
We are setting up the development environtment using the Processor SDK Linux for J7200 Version: 09_01_00 (which, as…
Part Number: J721EXCPXEVM Other Parts Discussed in Thread: TDA4VM Tool/software: When installing the new CCS V20.1.1 you are asked to select components to install. There are no components that I can see for Jacinto based SOCs ( TDA4VM) specifically. All…
Part Number: J721EXCPXEVM Tool/software: Is the following errata applicable to TI PSDK RTOS, which HW/SW component does it impact?
i2171 2-L SerDes: State Change Monitor interrupts are not available Details:
The 2-L SerDes State Change Monitor interrupt…
Part Number: J721EXCPXEVM
Hi,
My objective is to create a timer in U-Boot, it will be started during the booting process and if it expires (or completes the timeout period) then it should reset the CPU (that is restart the board). This is to ensure…