Part Number: J722SXH01EVM Tool/software: Hi,
I'm going to be designing my board based off the J722SXH01EVM and I'm going to be using a majority of the same components on this board. I currently got the schematics/board files and even the Schematic…
Part Number: J722SXH01EVM Hello. I referred to the Pbist example in the SDK and attempted to run Pbist in SBL, where SBL runs on the wkup-r5fss0-0 core. The execution cases of Pbist include SDL_PBIST_INST_MPU ~ SDL_PBIST_INST_MCU, totaling 12 instances…
Part Number: J722SXH01EVM
Tool/software:
How do I use the Fusion2 board with the J722SXH01EVM ?
When I try to run the single camera demo, I see the following error:
[MCU2_0] 76.844004 s: Error writing 0x01 to de-serializer(0x3d) register 0x4c…
Part Number: J722SXH01EVM Hi,
We are currently using the TI TDA4 platform, where we have successfully brought up our camera using the MAX96714 deserializer and MAX96717 serializer.
We now need to replace the MAX96714 with the MAX96716A deserializer…
Part Number: J722SXH01EVM
I defined one const pointer as Os_ReadyQueMg_Inf, and set some variables to it. But I found the address of Os_ReadyQueueMark_Core0 is 0x0000FFFF that is wrong, and the other three members's addresses are right.
static const…
Part Number: J722SXH01EVM We currently have a requirement to implement an overlay image drawing with transparency gradient. For example, for a line 15 pixels wide, we want to start at 20% opacity and increase by 20% every 3 pixels from left to right.…
Part Number: J722SXH01EVM Tool/software: Hi TI team,
Is the SDK for RTOS available for J722SXH01EVM ?
https://www.ti.com/tool/J722SXH01EVM
If not, which one is close enough for us to get started ?
We hope to have MiPi-CSI2 driver for freeRTOS…
Part Number: J722SXH01EVM Hi Team,
We are enabling a minimal UDS-over CAN-FD Diagnostic PoC on TDA4VEN EVM. The current kernel configuration shows ISOTP not set. How to enable this?
Best Regards
Part Number: J722SXH01EVM Hello,
We are trying to run the 'IPC RP Message Linux Echo' example application on the J722SXH01EVM. The freeRTOS projects for the remote-cores are available in the FreeRTOS SDK, but it is not clear what is the application…
Part Number: J722SXH01EVM Other Parts Discussed in Thread: ALP Hello, I see J722S Linux doesn't support DisplayPort. When I tried it, I didn't get a DisplayPort output either. Its only work with HDMI port.
What roadmap should be followed for DisplayPort…