Edo,
The purpose of the serverip line is to define where the dhcp command in u-boot should look for a TFTP server and attempt to load an image from. The DHCP protocol itself allows for various options and it seems your router may support one that allows…
I provided the http address to the Linux SDK (aka PSP) software package that you can download in my prior post. There is also a link to documentation on the processor wiki site to also help guide you in this process.
Part Number: SK-AM64B Hello everyone,
I am using an SK-AM64B ( SL#37221000333, ASSY#PROC100A(002) ) starter kit, and trying to boot it with the prebuilt linux image. I followed the official start guide for the board ( link ), downloaded the official…
Other Parts Discussed in Thread: AM3352 Dear Ti E2E Community
Am using ti sdk 8, am3352 processor, Am trying to understand the following from many days but still I don't understand w.r.t EDMA MCASP
I am trying to find out how to calculate the buffer_size…
Hi,
Please apply the patch attached on the linux kernel and rebuild (make linux, make linux_install). It should resolve the issue.
Regards
Shravan
Fullscreen
1157.0001-arm-dts-Update-timer-entries-for-remote-cores.patch.txt
Download…
Hi Fariya,
I am wondering if you face the same issue as the one mentioned in the thread "Linux/AM3352: Crypto driver crash on big files" you referred. The fix for that issue is in the latest Processor SDK Linux v5.2 which has kernel v4.14.79.
I attach…
Part Number: EVMK2GX Other Parts Discussed in Thread: SYSBIOS Tool/software: Code Composer Studio EVMK2GX bios_6_52_00_12 ccsv8 ipc_3_47_01_00 multiprocmgr_3_0_4_0 pdk_k2g_1_0_9 processor_sdk_rtos_k2g_4_03_00_05 ti-cgt-c6000_8.2.2 xdctools_3_50_03_33_core…
Ramakrishna,
Could you provide the link to where you downloaded the SDKs from? I have looked in the TI website and cannot find a SDK for DM814x MPU/DSP. I noticed that TMS320DM8146 , TMS320DM8147 and TMS320DM8148 are all new MPU/DSPs. I might…
Part Number: AM5728
Tool/software: Linux
Hi
I'm using AM572x custom board
and, I use GPMC MRAM (Multiplex mode)
MRAM: MR4A16BCMA35
U-Boot Command(md, mw) is working.
But, Linux Application can not use it.
Test MRAM memory [main] 99 Dev…