Part Number: 66AK2H06 Tool/software: Dear Sir,
I install ti-processor-sdk-linux-k2hk-evm-06.03.00.106 and run setup.sh under install directory.
it generates the file: arago-base-tisdk-image-k2hk-evm.ubi
However, I check k2hk_evm.sh, it need file arago-console…
Part Number: PROCESSOR-SDK-AM62X
Tool/software:
Hi, I'm trying to boot tiboot3.bin, tispl.bin and u-boot.img to EVM board over USB DFU: https://dev.ti.com/tirex/explore/node?node=A__AeVbwnGEP1NObR9gnw1lhA__AM62-ACADEMY__uiYMDcq__LATEST&placeholder…
Part Number: PROCESSOR-SDK-J722S Tool/software: Hi,TI experts!
I don't have a network router,so I want the development board to have a static IP address in TFTP stage and NFS stage.How to solve it?
And,how to change the default bootargs?Are there…
Part Number: PROCESSOR-SDK-AM64X Tool/software: Hello,
My customer is developing AM6xx.
May I have question about secure boot?
1.
I think if use SBL + **.appimage (MCU+SDK), all binary could encryption. (Security is x.509cert + code encryption)
But if…
Part Number: AM275-PROCESSOR-SDK Other Parts Discussed in Thread: SYSCONFIG , C7000-CGT Tool/software: According to the download page and documentation of FreeRTOS SDK for AM275, CCS v12x is recommended, but is it compatible with the latest CCS v20x? …
Part Number: PROCESSOR-SDK-J784S4
Tool/software:
Hello TI,
I am trying to use on-board debugger XDS110 on the TDA4 J784S4 follow guideline 7. CCS Setup for J784S4
I built debug mode for the DSP default application vx_app_rtos_linux_c7x_1.out on PSDK 0…
Part Number: PROCESSOR-SDK-AM64X Tool/software: I'm trying to use the CPSW and get an error in Udma_chOpen when it calls Sciclient_rmPsilPair. After a power cycle this works fine, but if I reload the debugger without a power cycle it fails because…
Part Number: PROCESSOR-SDK-AM335X Tool/software: Hi Ti experts,
I'm trying to get the Usb0 OTG functionality to work with a customized Linux kernel version 6.1, but I'm having trouble.
In old kernels, both the host and peripheral of the OTG function…
Hi,
manoj goud sudagoni said: SoC side set to 2500Base-X mode and there is a sync on the SoC side.
SoC side it is XAUI mode which is equivalent to 2500 Base-X mode with 8b/10b encoder and a lane rate of 3.125Gbps.
manoj goud sudagoni said: How i should…