Firstly, there is very little information in the post regarding the actual error itself, but based on previous customer questions regarding the Yocto errors question regarding ONNX, there are two links that can be useful.
Fixing the ONNX build error…
Ravi,
There are possibly two problems here:
If you are working behind a firewall, your proxy settings are not correctly configured to allow reaching some of the repositories (tiff, tensorflow-lite, websocketd - seem to fall under this category).
For…
Hi Seunghwan,
This question is answered recently, please see
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1072575/j7expcxevm-building-of-tisdk-fails-due-to-fetch-from-incorrect-git-repo-branch-name
and
https://e2e.ti.com/support…
Hi Haithem,
Lets separate the problems into two cases:
Base build of the SDK without the addition of libbpf
Addition of libbpf
Lets first get the build working for you, it seems like you need to pick one fix for the ONNX and make similar changes for…
Part Number: J721EXSOMXEVM Other Parts Discussed in Thread: J7EXPCXEVM , DRA829V , DRA829 , DRA821 Hi All,
I have J721EXSOMXEVM (SoM) & J721EXCP01EVM (baseboard) for evaluation purposes.
I want to test the PRU-ICSSG Linux driver/performance.
But as far…
Hi,
Yes, it is not supported in Software, even though the hardware does exist in the TDA4/DRA829.
The PWM pin is available in the expansion board (Gateway/Ethernet Switch Expansion): https://www.ti.com/tool/J7EXPCXEVM
The PWM signal exported on the board…
Part Number: PROCESSOR-SDK-AM64X I follow the directions from software-dl.ti.com/.../Release_Specific_Release_Notes.html
Using the ~/tisdk/configs/processor-sdk-linux/processor-sdk-linux-08_01_00.txt config and "MACHINE=am64xx-evm bitbake tisdk-base-image…
Part Number: TDA4VM Hello!
I'm going to test functions about ethernet using J721E_EVM board.
My development environment is the followings.
- Board : J721EXCPXEVM
- SOM : J721EXSOMXEVM
- Others : J7EXPCXEVM - Gateway/Ethernet switch expansion card
- SDK…