Part Number: MSP432P401R Tool/software: TI C/C++ Compiler I have an object file built with TI Arm compiler 16.9.4 LTS. I am using armofd from the same release to extract .debug_info and .debug_abbrev sections. DIE for a variable is missing the attribute…
I have a simple UART echo working with UART1 on the launchpad using Pin16 and 17. I've attached my .out (remove the.txt extension). You can load and run this using CCS. Since Pins 16 and 17 are JTAG pins TDO and TDI you'll have to use SWD (2-wire JTAG…
My setup was working fine for many weeks, then for some reason CCCSv4 is creashing when I load a program the second time.
This problem is not specific to the program that I am running.
If I reopen CCSv4 without power cycling the board I see errors either…