Part Number: ULN2003A Other Parts Discussed in Thread: L293D , Tool/software: WEBENCH® Design Tools Pls provide simulation file or spice model for ULN2003A and L293D.
I am not able to find anywhere.
Kindly do the needfull.
Regards,
Zeeshan
Hi Syed Zain Nasir,
To control the speed, change the duty cycle of the inputs.
For reference, please see the blog: e2e.ti.com/.../easy-cruise-control-for-brushed-motors-using-bemf
Part Number: L293D Tool/software: Linux Hi,
I'm a French student working on an RC autonomous car project. The first part of the project consists in controlling two DC motors using Pulse With Modulation. I use the L293D with a Raspberry Pi 3B+.
I have…
Part Number: LAUNCHXL-CC2640R2 Other Parts Discussed in Thread: CC2640 , L293D , ENERGIA Tool/software: Code Composer Studio Hi,
I have LAUNCHXL-CC2640R2
I have implemented project zero with BLE Scanner and able to control on board LEDs
I want to make…
Other Parts Discussed in Thread: L293D , DRV8816 , DRV8871 , DRV8870 , DRV8801 , DRV8872 , DRV8841 , DRV8844 Hi,
I am looking for an Integrated Motor Drive solution for out DC motor. The Specs are simple, the motors are 12 V DC motor with 1.8A RMS current draw…
Part Number: L293D Other Parts Discussed in Thread: DRV8844 I am using the L293D to create zero crossing signals. It does this without problems. I want to make my design smaller and I am looking for a replacement. I have included the current circuit. …
Part Number: DRV8812 Other Parts Discussed in Thread: L293D Hi,
To drive DC motor with 24V and nominal current is 600mA (1.2 A peak), we have selected DRV8812 as alternate part for L293D (from ST).
As L293D internal clamping diode, which is not available…
Other Parts Discussed in Thread: L293D , ULN2003A , ULN2004A , ENERGIA Hello,
I have a L293D that is powered by a LiPo battery/ power boost combination ( www.adafruit.com/.../1903) . This combination outputs 5v, which is my system's Vcc. Ultimately, I am trying…