Part Number: LAUNCHXL-CC1312R1
Hello,
I like to modify the matching network of the LAUNCHXL-CC1312R1 to optimize its output power and sensitivity for 434 MHz operation.
According to “CC13xx/CC26xx Hardware Configuration and PCB Design Considerations…
Part Number: LAUNCHXL-CC1312R1 Hey,
I use CC1312R1 and I've noticed that sometimes when i turn off the voltage supply, the FLASH erase itself.
I had some research and it occurs because the CS (Chip select) is trying to write while VCC is going down…
Part Number: LAUNCHXL-CC1312R1 I have a project that I import that when I build shows: Product com.ti.SIMPLELINK_CC13XX_CC26XX_SDK v7.10.2.23 is not currently installed. I did install the SDK SimpleLink Low Power F2 SDK 7.10.02.23. Is this the correct…
Part Number: LAUNCHXL-CC1312R1 Other Parts Discussed in Thread: SYSCONFIG Tool/software: I want to use flash memory from 0x0 until 0x2FFFF for my program, 0x30000 until 0x31FFF for time value, 0x32000 until 0x57FFF for log value.
i already set the…
Part Number: LAUNCHXL-CC1312R1 Hi guys:
I use two pieces of CC1312R1,One as a collector and the other as a sensor, Now the business has been completed.Only the load function is missing.
The load function provided in the routine is based on the coprocessor…
Part Number: LAUNCHXL-CC1312R1 Other Parts Discussed in Thread: SYSBIOS Can i know the example code of combine of Queue and Task (<ti/sysbios/knl/Queue.h> and <ti/sysbios/knl/Task.h>)?
The condition is: two or more task, each task will communicate,…
Part Number: LAUNCHXL-CC1312R1 Hi TI team, I have a general question about NVS implementation to read / write to external flash (Macronix MX25R)
What is the rule of thumb using NVS_open() and NVS_close().
For each read transaction should I call NVS_open…
Part Number: LAUNCHXL-CC1312R1 We develop a code for certificate verification on our devices. We need an example of how to use the API in simplelink_cc13xx_cc26xx_sdk_7_10_00_63_eng\source\ti\drivers\cryptoutils\cryptokey\CryptoKeyKeyStore_PSA.h to perform…
Part Number: LAUNCHXL-CC1312R1 Hi team,
My customer would like to configure the RF frequency to 1200MHz, but it seems like CCS doesn't allow to do it from the figure below. Are there any ways to configure RF frequency to 1200MHz?
Best regards, …
Part Number: LAUNCHXL-CC1312R1 Tool/software: I would like to access the serial number of LAUNCHXL-CC1312R JTAG debugger in run time from the active application. Is there a solution?
I would like to use them as a unique ID in a network.
For some reason…