Part Number: LAUNCHXL-F280039C Hi Team,
I would like to check if we can put the LAUNCHXL-F280039C in 85C chamber for testing?
What is the Tamb(max) that LAUNCHXL-F280039C can use?
Regards,
Roy
Hello,
The Altium design files are available on the TI tool page https://www.ti.com/tool/LAUNCHXL-F280039C and C2000Ware repo: C:\ti\c2000\C2000Ware_5_05_00_00\boards\LaunchPads\LAUNCHXL-F280039C\RevA\design files
Part Number: LAUNCHXL-F280039C I have purchased the launchpad F280039C and DRV8323RS in order to learn motor control with the universal motor control lab. I made all the hardware modifications in the guide (spruj26) except populating c9/c10/c11 with 47nF…
Part Number: LAUNCHXL-F280039C I am currently working on a bootloader for the LAUNCHXL-F280039C board. First, I wrote a customized bootloader in flash memory, and then I wrote the application code at a different flash memory location. The application…
Part Number: LAUNCHXL-F280039C Other Parts Discussed in Thread: C2000WARE I'm using LAUNCHXL-F280039C board with CCS V20.4.0.13, and also installed C2000Ware_6_00_01_00.
I connected two these EVB boards on J14 (CAN A), all 3 pins, and I'm using an example…
Part Number: LAUNCHXL-F280039C Other Parts Discussed in Thread: TPS55289EVM , C2000WARE Tool/software:
Hi
I have a Lunchpad LAUNCHXL-F280039C. I want to use the I2C interface to control TPS55289EVM to generate a 0- 22V voltage. Is it feasible? Unfortunately…
Part Number: LAUNCHXL-F280039C Other Parts Discussed in Thread: C2000WARE Tool/software: Currently working on -LAUNCHXL-F280039C bootloader, so I need some details about -LAUNCHXL-F280039C board. please find the quires below.
1.Is custom bootloader…
Joe Arcuri said: Using CCS Version 20.5.0 (20.5.0.883) and my Mac is an M4 Pro with Tahoe Version 26.3.1(a).
I tried a similar environment. The only difference for me was I was using a MacBook Air M1. It worked fine
One thing to check is to make sure…
Part Number: LAUNCHXL-F280039C Other Parts Discussed in Thread: C2000WARE
Hi,
I'm using LAUNCHXL-F280039C board with CCS V20.4.0.13, and also installed C2000Ware_6_00_01_00.
I loaded and ran Debug on an example project, led_ex1_blinky, without any…
Part Number: LAUNCHXL-F280039C Other Parts Discussed in Thread: C2000WARE , TMS320F280039C I'm using LAUNCHXL-F280039C board with CCS V20.4.0.13, and also installed C2000Ware_6_00_01_00.
I loaded an example, gpio_ex2_toggle, project from CCS. After…