Hi ZR,
"the following is the output of board. it is obvious that 3 stages are done: UBL->uboot->linux->UBL(loop)"
I do not think so. Your flow seems to stuck at "Uncompressing Linux ...." stage. This is before linux stage. The flow stuck at the…
Other Parts Discussed in Thread: LINUXDVSDK-DV Hello.
Our main task is video transcoding and transrating. We need to process as more channels as posssible by one device.
Currently we are using DM8168. It can transcode 16 720x576@25fps or 3 1920x1080…
Other Parts Discussed in Thread: TVP5158 , LINUXDVSDK-DV Hi,
I am following the TVP5158 EVM User's guide and under section 7.2.1 it says to "Unzip the UBL_DM646x_NAND_675_324.zip archive file onto the PC's local hard drive."
I can not find this .zip…
Check example code at Spectrum Digital site (at following DM6467 EVM support page) and see if there is Video port display example:
http://support.spectrumdigital.com/boards/evmdm6467
Also, look at DM6467 DVSDK, which has video port driver and some…
Hi Fikret,
would you be willing to try and download the latest DVSDK version?
http://www.ti.com/tool/linuxdvsdk-dv
Or is these examples:
http://www.ti.com/tool/c64xpluscodecs
http://www.ti.com/tool/demoapp-dm6437
Another tip, the error you…
Other Parts Discussed in Thread: OMAP-L137 , LINUXSDK-OMAPL137 , TMS320DM6446 , LINUXDVSDK-DV i need new gcc to use the stackguard technique or plz let me know how to use some other stack corruption technique
my gcc is too old
gcc version 3.4.3…
Other Parts Discussed in Thread: LINUXDVSDK-DV Hi,
We have buy a DM368 IPNC from APPRO,but They have not supply develope SDK. And also have not find DM368 DVSDK in WIKI.
And I want to know when DM368 DVSDK can download.
Thanks a lot!
Other Parts Discussed in Thread: LINUXDVSDK-DV
Where would I find a page which clearly defines the differences between the PSP, LSP, and DVSDK for the DM355?
I've looked at this page: http://wiki.davincidsp.com/index.php/PSP_Introduction_and_Product_FAQ…
Other Parts Discussed in Thread: LINUXDVSDK-DV Hi,
When I run the NDK on the 3 cores of the C6474 EVM, I see strange behavior. If I use the default hardcoded MAC addresses (00-01-02-03-04-05, 10-11-12-13-14-15, 21-22-23-24-25), I can ping the devices…
Other Parts Discussed in Thread: OMAP3530 , LINUXDVSDK-DV , CCSTUDIO (EVM6446)
I want to write an algorithm of video processing in DSP, but I don't know how to begin with: I have two questions:
1. Which system should I select: Linux or Windows? I…