Part Number: LM117HVQML-SP Hi team
Is a SPICE model available for the LM117HVQML-SP.
I've checked the product folder and all of the usual places but haven't found on yet.
Thanks!
Jim B
Part Number: LM117HVQML-SP Suffix A of part number 5962R9951705V9A (LM117H MDE) means it is hot solder dip lead finish. According to TI web site the component is Green (RoHS & no Sb/Br).
What is the plating of 5962R9951705V9A terminals, materials and…
Part Number: LM117HVQML Hi,
I'm using on a space application LM117HVGW-QML chips.
I need some information about internal thermal protection circuitry that is evoked in datasheet (SNVS357D– MARCH2006– REVISED APRIL2013).
* Which type of temperature…
Part Number: LM117HVQML Hello all,
The TI datasheet page 2 http://www.ti.com/lit/ds/symlink/lm117hvqml.pdf , Figure 3 shows the LM117HVGW-QML 16-Pin CFP pin connections.
It also has a statement that says "For the CFP device to function properly, the…
Part Number: LM117HVQML-SP Hi everybody,
I'm not managing to find mass data about the LM117HVQML-SP, in particular the SKU with part number 5962R0722902VZA. In the respective webpage ( http://www.ti.com/quality/docs/materialcontentsearch.tsp?partNumber…
Part Number: LM117HVQML-SP Other Parts Discussed in Thread: LM117QML , LM117QML-SP hello
i have a few more questions about regulator LM117H MDE.
1. what is the thermal resistance of LM117H MDE as it in DIE configuration ?
2.is the junction temperature…
Part Number: LM117HVQML-SP Hi,
I'd like to have references regarding the flight heritage of the component in object (flight hours, missions, missions profiles etc.).
Thanks in advance,
EF
Part Number: LM117HVQML-SP Hello
My question is regarding the die version of the part: LM117H MDE (not for the packaged part)
Can you please advise what is the max. current at Tj=105C
At the following setup:
Vin = 10.3V, Vout = 8V
and please…
Other Parts Discussed in Thread: LM117HVQML-SP Hi~
Our customer checking about LM117HVQML-SP device.
If see datasheet, it mentioned 5962# Part number.
What is different that 5962R0722901VXA, 5962R0722902VXA, 5962R0722961VXA ??
Please reply as…
Part Number: LM117HVQML Tool/software: Thank you for contacting us. Please let me know again.
If the frequency is 1MHz to 400MHz and the output capacitor is 6000μF, is it possible that the PSRR will fall below 10dB?
Also, if it falls below 10dB, how…