Is the metal body of the voltage regulator LM337H/NOPB may cause the short circuit if it touches with other components/metal components? Because, from our understanding, the body of the component should be inductive, and not conductive. Can you please check…
Part Number: LM337-N-MIL In our Amplifier application, the Voltage regulator of LM337H/NOPB is touching the metal lid of the body casing, it then causes the failure: short circuit between this voltage regulator LM337H/NOPB and the lid body casing. It results…
Part Number: LM317-N-MIL
Hi Experts,
Good day. I am reaching out to guide us completing the information requested by a known Cx:
OPN
MIN INPUT
MAX INPUT
LM317K STEEL/NOPB
?
?
LM350K STEEL/NOPB
?
?
LM317HVK STEEL/NOPB
?
?
LM79L05ACM/NOPB
? …
Hi Jimmy,
My mistake I used Ghz instead of Gbps.
It looks like with 157 ps/inch you are seeing 0.157 ps/mil and with an intra pair skew of 3.5ps that mean that if you divide the intra-pair skew we can see that 3.5/0.157 = 22.2 mils difference between…
Tool/software: hello pls confirm p/n LM117HVK is no more available
also available the MIL PART / 883
that means it is exactly the same product but with MILITARY TEST correct?
exist a cross reference between the two parts'?
Part Number: LM301A-N Hi,
I found the description about the slew rate of LM301A-N in D/S page1(FEATURES) and Page13(Figure39 and 40).
Does anyone have the operating characteristic data of slew rate of LM301A-N at specified conditions? (like page7 in TL031…
Part Number: LM350-N-MIL Other Parts Discussed in Thread: LM350-N , , LM350A Hello team.
The TI product page says for the LM350-N-MIL device the data sheet applies to both LM350-N and LM350-N-MIL.
In the data sheet Absolute Maximum Ratings it’s not clear…
Hi Vaibhav,
1. I'm reading the Interrupt count and Log address register (0x000A) and Master Status and reset register (0x0001) using direct access method in which we are not using any MAP register.
2. We are reading Remote terminal operational status…
Part Number: SN55115 TI datasheet for part SN55115 also lists JM38510/10404BEA as an available part under this datasheet. When dealing with part schematics, we found that the diagram in the TI datasheet looks different from the one in the mil spec MIL-M…
Part Number: DP83561-SP Tool/software: To whom It May Concern,
Hope you're well.
Please allow me to submit inquiry regarding Static Burn-In for device below?
P/N:5962F2021601VXC
Date Code: 2113B
Per SMD, it says "Static Burn-In test shall be performed…