Part Number: LM25149
Hi, I am working on a design involving TI's LM25149 buck regulator IC to convert a 12V input voltage (5-14V range) down to 3.8V with a peak current of 3.5A. Average load current is 1A but short bursts up to 3.2A are expected. The…
Part Number: MSPM0G3507 Hi
The documents for MSPM0 G-Series 80MHz Microcontrollers and MSPM0G350x Mixed-Signal Microcontrollers with CAN-FD Interface do not mention the selection of an External 4MHz to 48MHz crystal oscillator (HFXT).
The MSPM0G3507…
Hi John,
We are building liquid immersion system. Liquid is suppose to full submerge the system. If liquid level goes low, that is a concern as system will get hot.
The measurements which we shared are the one in air mode. We want to trigger if Capacitance…
Part Number: TPS61169 Other Parts Discussed in Thread: TPS61163A , TPS61163 , LM3697 What is the best driver to use with 36 of the attached top-emitting SMD LEDs and a 3.7 V power source at about 20 mA? Cost is a major if not the determining factor. Thank…
Part Number: SN74ALVC164245 Hello,
I am looking for the following parameters of the component SN74ALVC164245DGGR:
Thermal resistance junction to case
Thermal resistance case to ambiant
Thermal resistance junction to ambiant
I was not able…
Hi Simba,
We have the IBIS-AMI model available, within the model there are Tx and Rx package s-parameter models that can be used. We don't have s-parameter models for settings through the redriver, only the IBIS-AMI model is available for modeling the…
Hi Remi,
It's generally mentioned in the datasheet or on the website, but there've been some updates to the site and it's missing. However, we've highlighted this issue to the backend team, and they are working on it, it may take some time.
But you…
Part Number: TPS7H1101-SP Other Parts Discussed in Thread: TPS7H1101A-SP Here in Mason Ohio at Rocketdyne (formally L3Harris), we are using the TPS7H1101A-SP to regulate out a 1.05V core voltage rail from a 3.3V rail.
We are coming up to an issue…
Part Number: ADC12DJ3200
Dear Texas Instruments Support Team,
I hope this message finds you well.
We designed in your 5962F1820901VYF (ADC12DJ3200QML‑SP) device for use by our customer in an aerospace application.
We understand that this device…