Chaitanya,
The best one we have is the LM3532 with the ambient light sensor input. This can only get up to 30mA per channel. We do have others that have more current (LP8556), but no ALS.
Thanks
Travis
Unfortunately this is the only plastic packaged device with the dual PWM controls. There is the LM3532 which has 2x PWM's, but is in a chip scale package and requires I2C. The other possibility is to add an extra diode + capacitor boost circuit to the…
Other Parts Discussed in Thread: LM3532 Hi,
I'm looking to use the LM3532 but need more than the 29.8mA available per string. Is it feasible to short say ILED1 and ILED2 to get double this current?
Thanks,
Paul
Part Number: CC3351
Tool/software:
We encountered the failure unable to get hci0 interface via BLE over SDIO.
Please check the following log.
[22/08/2025 15:24:56.767] HWTEST:root@bsh-smm-m2b [~]# echo 8 > /proc/sys/kernel/printk
[22/08/2025…
I have a similar issue.. can someone please respond to this?
here is my log
Uncompressing Linux... done, booting the kernel. <6>Initializing cgroup subsys cpu <5>Linux version 3.0.8 (ravi@ravi) (gcc version 4.4.3 (GCC) ) #3 SMP PREEMPT Sat Jul…