Part Number: LM4050-N-Q1 Could you please help confirm below two questions? Thank you!
First please check and confirm below products are NOT subject to China’s dual-use regulations.
Second please check and confirm that Chinese-made synthetic diamonds…
Part Number: LM4050-N Tool/software: Hello,
I see that LM4050 Q AEM3-8.2/NOPB is obsolete with LM4050AEM3-8.2/NOPB as the recommended pin-to-pin alternative.
Is there a datasheet for the obsolete LM4050 Q AEM3-8.2/NOPB? I do not see this MPN listed…
Part Number: LM4050-N-Q1 Tool/software: Hi there, a customer is trying to use this part, and needs some details around the ACTUAL qual testing that was done for LM4050QAIM3-2.5/NOPB:
Looking at the quality report for this specific device (p/n LM4050QAIM3…
Part Number: LM4050-N-Q1 Tool/software: Hi expert,
I'm looking for help with differences between LM4050QAEM3-2.5/NOPB and LM4050QAEM3X2.5/NOPB.
Is there any difference between these two part numbers?
Hope for your reply. Thanks!
Vickie Wu
Part Number: LM4050-N-Q1 May I ask whether the chip can guarantee that its output meets the accuracy of 0.1% at 25℃ under the following conditions? The chip current in our application is approximately 0.8~0.9 mA. Thanks
Part Number: LM4050-N-Q1 Other Parts Discussed in Thread: LM4040 , Hi team,
My customer use LM4050 to replace Diodes LM4040.
Input voltage is 6.5V, input resistor is 150 ohm. They connect 2 22uF capacitor at output node.
In Diodes LM 4040's experiment…
Part Number: LM4050-N-Q1 Hi team,
Could you pls help share below Ir=1mA is spec at what temperature range? Datasheet has list 25C and full temp range spec for Ir=100uA, but didnt specify it clearly for Ir=10mA/1mA
Thank you
Scarlett
Part Number: LM4050-N Hello,
In order to calculate the failure rate of products using this part, could you please provide information on the failure rate of the LM4050BEM3-2.5/NOPB, as well as MTBF and FIT values?
Thank you,
Keisuke IKEMORI
Part Number: TINA-TI Other Parts Discussed in Thread: LM4050-N , TINA-TI I am looking for a simulation model for LM4050-N in the 5 Volt Variant ( www.ti.com/.../LM4050-N ) and found a reference design: www.ti.com/.../snom432 and a model: www.ti.com/.…
Part Number: LM4050-N-Q1
Hi Expert,
My customer is doing the FuSa analysis for their system. LM4050 is used in this project. Can you help fill the component type to the excel for LM4050 based on SN29500?
I saw there have SN29500 category in FuSa…