Part Number: LM5013-Q1 Other Parts Discussed in Thread: LM5013 Tool/software: Hi Expert,
Customer is considering lm5013-Q1. They have concern about power assumption. They require the current assumption of lm5013-Q1 is lower than 30uA when the 5V output…
Part Number: LM5013 Tool/software: Hi,
The customer has the following two problems when using this chip design, please help troubleshoot the problems, the schematic design is as follows;
1. The customer found that there will be a whistle when the circuit…
Part Number: LM5013-Q1
Tool/software:
Hi all, I urgentlty need to order some new PCB's for a project but the circuitry uses teh LM5103-Q1. I can not get any stock of this from anywhere at the moment. Is there anything that could be a drop in replacement…
Part Number: LM5013 Tool/software: Dear Experts,
The circuit diagram is as follows.When powered on with a 48V lithium battery, the chip works normally; When using a 56V lithium battery for power on, the VIN and EN pins were burned out. Upon checking…
Part Number: LM5013 Tool/software: hi team,
my customer wants to use lm5013 to run at Vin:36V, Vo:12V with the constant current 3A. The SCH and PCB is as below.
The solution can only run to 2.7A and the temp of the chip will rise to 110℃.When they run…
Part Number: LM5013-Q1 Tool/software: We had built a dual 5/5.3V supply to be fed from a 22.2V-75V input, the design was verified here. https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/1389988/lm5013-q1-design…
Part Number: LM5013 Tool/software: Hi team,
This is Gree FAE Ryker. Recently I have promoted LM5013 to Gree R&D and DIN in their schematic. But I found there is not sample in TI Samples Internal | Homepage as below. So do we have other way to get the…