Part Number: LM5141-Q1 Tool/software: Hello Team,
We are using the LM5141-Q1 in our design for converting 12V input to 3.3V @ 10A output. The schematic is attached below. Kindly request your expert review and comments on the implementation. Key Specs…
Part Number: LM5141-Q1 Hello team,
I'd like to use LM5141-Q1 to design a single BUCK with:
Vin: 4V~36V
Vout: 3.3V
Iout: 14A
I understand that t he output current is determined by the power stage componnets (MOSFET and inductor), not the…
Part Number: LM5141 Other Parts Discussed in Thread: AM62A7 , SK-AM62A-LP , LM25141 , CSD18563Q5A Dear TI experts,
My customer using LM5141 to operate AM62A7.
They designed their schematic based on SK-AM62A-LP EVM schematic.
And they had no problem…
Part Number: SK-AM62A-LP Other Parts Discussed in Thread: AM62A7 , AM62A3 , LM5141 Tool/software: Hi, Dear Expert
Customer reference our EVK ( AM62A7 / AM62A3 LOW POWER STARTER KIT SK ), and start board design.
EVK power block as below :
Follow…
Part Number: LM5141 I increased the HS shut down resistor, why can I also reduce SW ringing.IS SW ring be related to the High side Mosfet shutdown speed?
Part Number: LM5141-Q1 Other Parts Discussed in Thread: LM5141 , LM25143-Q1 , , LM5143A-Q1 , LM25148-Q1 , LM5148-Q1 , LM25141-Q1 , LM25149 Hello team,
I found the max current LM5141 can support is 30A in the Data sheet , but I have question w.r.t the…
Part Number: LM5141 Other Parts Discussed in Thread: LM5146 , CSD17308Q3 , CSD18532Q5B , CSD18534Q5A Hi every expert, my design is as below.
LM5141QRGERQ1 design:
switch power supply: input 24V
battery supply:14V-16.8V
output voltage12V,output…
Part Number: LM5141 Other Parts Discussed in Thread: LM5146 I am working on a project using the LM5141 as the controller which feeds HO/HOL and LO/LOL to two gate drivers that drive two mosfets each. At first I was thinking that I need both gate drivers…
Part Number: LM5141 Hi,
What is the current drawn by LM5141 during the light load condition and in the design the DEMB ( diode emulation ) pin pulled High for the continues operation (FPWM).
Part Number: LM5141-Q1 Hi team,
I want to use WeBench to simulate load transient response for LM5141-Q1. But the simulation failed as shown below
How can I fix this?
Regards,
Bengi Long