Part Number: LM63 Dear Team,
We found the minimum hold time requirement changed to 0sec in SMBus 3.0, which is aligned with I2C hold time requirement.
Is the LM63 compatible with SMBus 3.0?
We also followed your previous comments to perform…
Part Number: LM63 Other Parts Discussed in Thread: 66AK2G12 , Hi,
We are using LM63 as our temperature and fan control chip. There are many sysfs files that the lm63.c driver can export. However, on our system which uses TI 66AK2G12 CPU, only one, temp1_input…
Part Number: LM63 Dear Team,
We use LM63CIMA on our WiFi AP product to control the fan, and we use the I2C interface to control the LM63CIMA.
But from the datasheet, LM63CIMA only supports SMBus, and there are some differences in timing spec between…
Part Number: LM63 Dear Team,
It is about SMBus timing, the problem description is as follows: 1. Does this material comply with the SMBus 2.0 or 3.0 specification? 2. If tHD;DAT (ns) is smaller than the specification, is there any suggested way to…
Part Number: LM63 Hi Expert,
I have some questions I would like to ask. If my customer’s application does not connect to the SMBus on the host side (it needs an external EEPROM), is there a public version of the line that I can refer to?
If you have…
Part Number: LM63 Hi expert,
Customer used LM63 and have some issues about the driver.
They can read I2C device(4C).
But below commands are all NACK.
i2cset -f -y 0 0x4c 0x4D 0x0d i2cset -f -y 0 0x4c 0x4c 0x04 =>> rpm = 1075 Run: i2cset -f …
Part Number: 66AK2G12 Other Parts Discussed in Thread: LM63 Hi,
We are using LM63 as our temperature sensor and fan control chip. There are many sysfs files that the lm63.c driver can export. However, on our system which uses TI 66AK2G12 CPU, only one…
Part Number: LM63 Dear Team,
Does TI / LM63CIMA could be compatible with SMBUS 3.0? Because We found the SMBUS spec of TI / LM63CIMA is SMBUS 2.0.
Many Thanks,
Jimmy
Part Number: LM63 Hi team,
Customer wants to use a fan controller to control 2 fans, now they goes with MAX31760 , do you get any recommendation for this?
Thanks and Best Regards,
Will