Part Number: LM63625-Q1 Problem Description
Our design utilizes the LM63625DQDRRRQ1 to convert a 24 V input to a 16.8 V output. The device initially performed as expected. However, during a boot cycle test conducted under no-load conditions (16.8 V…
Part Number: LM63625-Q1 Dear sir,
I'm working with LM63625DQDRRRQ1(RT = GND; fSW = 2.1MHz).
I'm not sure when the speed spectrum feature will work on the above device. Is there a specific part number? Does the function work regardless of the operating…
Part Number: LM63625-Q1 Tool/software: Dear TI Assembly Engineers,
The package outline of LM63625DQDRRRQ1 is WSON (DRR) | 12. www.ti.com/.../mpss085a.pdf
We would like to confirm actual measurement data for the clearance (standoff) between the leads…
Part Number: LM63625-Q1 Tool/software: Hi,
My customer has asked about the accuracy of the 5 V output of this IC. Currently, we are operating at a switching frequency of 400 kHz. However, the line and load regulation at this frequency is not provided…
Part Number: LM63625-Q1 Tool/software: Hello
I need a stepdown converter from 24v to 12v to power my circuit. The 24v is coming from Fuse box of the truck. Could you please advice for source rail requirements on the lm63625 ? Could you provide me a…
Part Number: LM63625-Q1 Tool/software: Hello experts,
What is the short circuit protection time for LM63625-Q1?
Customer would like to know the time from Short applied to output voltage down.
Thanks,
Kento
Part Number: LM63625-Q1 Tool/software: Hi team,
I would like to ask the following two questions about the VIN pin and reset pin for LM63625DQPWPRQ1.
① :If the LM63625DQPWPRQ1's 12-, 13-pin VIN is unpowered and the 8-pin reset is pulled up externally…
Part Number: LM63625-Q1 Tool/software: Dear TI Product Engineers and Assembly Engineers,
The LM63625DQDRRRQ1 has an exposed pad on the back of the product to improve heat dissipation. The customer is concerned about the effect the solder joint area…
Part Number: LM63625-Q1 Tool/software: Hi here, We use LM63625DQ-Q1 buck converter for to supply a discontinues load (2.5A(pulse)/8V) two high-power IR LEDs, which will be ON for 3.33ms in every 33ms cycle. The current rating for the regulator is 2.5A…
Part Number: LM63625-Q1 Tool/software: HI team,
Regarding LM63625DQPWPRQ1, FuSa document shows that the FIT is 17(IEC TR 62380/ ISO26262) or 25(SN 29500-2).
But the estimator shows very low FIT. I'm suspecting that applied mission profile is different…