Part Number: LM63625-Q1 Tool/software: Dear TI Assembly Engineers,
The package outline of LM63625DQDRRRQ1 is WSON (DRR) | 12. www.ti.com/.../mpss085a.pdf
We would like to confirm actual measurement data for the clearance (standoff) between the leads…
Part Number: LM63625-Q1 Tool/software: Hi,
My customer has asked about the accuracy of the 5 V output of this IC. Currently, we are operating at a switching frequency of 400 kHz. However, the line and load regulation at this frequency is not provided…
Part Number: LM63625-Q1 Tool/software: Hi team,
I would like to ask the following two questions about the VIN pin and reset pin for LM63625DQPWPRQ1.
① :If the LM63625DQPWPRQ1's 12-, 13-pin VIN is unpowered and the 8-pin reset is pulled up externally…
Part Number: LM63625-Q1 Tool/software: Hello experts,
What is the short circuit protection time for LM63625-Q1?
Customer would like to know the time from Short applied to output voltage down.
Thanks,
Kento
Part Number: LM63625-Q1 Tool/software: Hello
I need a stepdown converter from 24v to 12v to power my circuit. The 24v is coming from Fuse box of the truck. Could you please advice for source rail requirements on the lm63625 ? Could you provide me a…
Part Number: LM63625-Q1 Tool/software: Dear TI Product Engineers and Assembly Engineers,
The LM63625DQDRRRQ1 has an exposed pad on the back of the product to improve heat dissipation. The customer is concerned about the effect the solder joint area…
Part Number: LM63625-Q1 Tool/software: Hi here, We use LM63625DQ-Q1 buck converter for to supply a discontinues load (2.5A(pulse)/8V) two high-power IR LEDs, which will be ON for 3.33ms in every 33ms cycle. The current rating for the regulator is 2.5A…
Part Number: LM63625-Q1 Tool/software: HI team,
Regarding LM63625DQPWPRQ1, FuSa document shows that the FIT is 17(IEC TR 62380/ ISO26262) or 25(SN 29500-2).
But the estimator shows very low FIT. I'm suspecting that applied mission profile is different…
Part Number: LM63625-Q1 Tool/software: Hi Team,
The datasheet recommend the ripple ratio is setting as 20%-40%. I am wondering if it can set as 50% if we pass the RA test, time domain test and bode plot in worse condition.
Below are articles that…
Part Number: LM63625-Q1 Tool/software: Hi team,
I have a question about Vfb_5V (Feedback Voltage) spec in the datasheet EE table.
The test condition is specified as Vin=5.5V-Max operating Vin.
When Vin drops below 5.5V and the device fall into dropout…