Thanks for the answers. One last question, for the JTAG, do you have any recommendation that I can use aside from Eval Board? Like Xilinx or XDS200?
And if I use XDS200, I should use CCS to download the flash. Is there any possibilities that I can use…
Hello Jonathan,
From what I have gathered, TI handles return processes for boards shipped through our TI.com eStore. Not for other distributors. That Mouser is requesting TI to look into this has not come up before.
I would ask you to do one more…
Deepanraj Anbarasan said: Please let us know how to program the binary file
Do you want to write your own program for the PC, or use an existing one? You can use LMFlashProgrammer to load a binary file to a device using the serial boot loader. If you…
Hello Richard,
When you check for the DFU being available, are you using LMFlashProgrammer for that? Does it show no device listed under "Manual Configuration", "Interace = USB DFU"?
That the device shows up as a Stellaris Device Firmware Upgrade…
Renat - If you want to try reloading your FW, please follow the instructions below. Again, this is assuming the EVM firmware has been erased.
1. Download and install LM Flash Programmer from
2. Run LM Flash Programmer
3. Under the Configuration…
Hi,
First I assume you run the usb_stick_update first which is a usb bootloader to load the usb_stick_demo from your usb stick. Is this correct? Can you please check if the usb_stick_demo.bin which is renamed to FIRMWARE.BIN is properly loaded into…
Hello Vivian,
Before a replacement can be issued, please have them do the following:
1) Download these drivers onto the PC being used: https://www.ti.com/tool/STELLARIS_ICDI_DRIVERS
2) Open Device Manager in Windows and look if the Stellaris In…
Thanks for the reply. However, I have looked at lmflashprogrammer, and I don't think it is what I need. The problem is that the embedded system that the Tiva part is installed in does not have an interface that lmflashprogrammer understands. It has an…
Hi Marius,
Welcome to the E2E forum! Always be careful with button presses. What happened is you erased the firmware for the micro. You can reinstall the firmware by following the the steps below:
Download and install LM Flash Programmer from https…