Part Number: TLV320AIC3101
Hello
My customer use TLV320AIC3101 at next model portable recoder ( soon in mass production) as before.
This time customer use very low noise pin mic ( floor noise < -120dB).
At this point they found some qurious…
Part Number: TDA4VM-Q1 Hi, TI experts,
After refer the thread we had post before: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1343208/tda4vm-q1-tda4vm-q1-tda4vm88t5balfq1-sr1-1-hs-fs-how-to-build-and-flash-keywriter …
Hello,
Thank you for your answer and your support,
Sorry for the delay in responding, but I wanted to repeat operations properly.
The problem was identified initially with an Ubuntu 18.04 installation but with a VMWare Fusion virtual machine.
…
Hi, I think the problem may be firmware version of USB2ANY. Please use version 1_19_0_0. By some unknown reason, version later than that can't support this EVM. You can take below link as reference, which has similar issue. e2e.ti.com/.../690036 Any further…
Tool/software: Linux
Hello, I try to build SDK fort processor-sdk-04.03.00.05-config.txt, but result is - build error when ti-llvm3.6_3.6.bb processed.
In related issue used CCS, but i use standalone gcc-linaro-6.2.1-2016.11-x86_64_arm-linux-gnueabihf…
Hi Board designers,
The below links are a quick reference to the collaterals that can be referred when starting a custom design.
Device Selection and features
Product Page
https://www.ti.com/product/AM625
Note:
Any AM62x device implemented…
Hello Justin,
The re-flashing process was successful, nevertheless the same issue happens with the sampling/measurment time.
I have compared a "fresh" EVM with an "upgraded firmware" EVM, please check the attached log files. Data streaming was done…
Hello Scott,
Another E2E user just experienced a similar issue: e2e.ti.com/.../625231
Note that your best option is to put the device into BSL mode and reload the firmware that is included in the 1.9.2 version. The typical location of this file is…
Hi Matt,
Attached below is the updated excel file with my recommended component selections. I'll explain the design choices that were made as well:
1. Switching Frequency - Your selection of 1400kHz is a reasonable selection. This "high" switching…
Part Number: CC2538 Tool/software: Hi team,
My customer would like to ask about the SPI.
The cc2538 is used as a slave for SPI communication, but there is a problem when communicating at 5MHz.
The attached User’s Guide does not seem to describe…