Part Number: LMH0070 Hi expert,
What is the voltage at RSET pin? We would like to know this information so that We are going to consider the voltage and wattage ratings when selecting the 8.06k ohm resistance to be connected to RSET pin.
Part Number: LMH0070
Hi expert,
We want to confirm about the handling of unused pins. We are not using the following pins and are handling them as described below. Is it correct to assume there are no particular issues?
RSVH_H: Pull High via 5 kohm…
Part Number: LMH0070 Hi expert,
Is there a possibility that current could leak from VDD3V3 to VDD2V5 inside the LMH0070 when the power is turned on? As described on Datasheet Page 9, the power is applied in the order of 3.3V first, then 2.5V, but it…
Part Number: LMH0070 Tool/software: Hi Team,
We are using SD- SDI converter LMH0070SQE/NOPB part in our project. we would like to know that, What is the current consumption of pin 28 (VDDPLL) .
Regards,
Sanju
Part Number: LMH0070 Tool/software: Hi expert,
What is the parasitic capacitance value of TXOUT+ and TXOUT- pin? (it's OK even if the value is approximate.)
We are planning to do Return Loss simulation and are investigating electrical characteristics…
Part Number: LMH0070 Other Parts Discussed in Thread: LMH0303 Tool/software: Hi expert,
Is the S-parameter file(.s4p) for LMH0070SQE/NOPB available?
We are planning to do Return Loss simulation and are looking for this file.
Part Number: LMH0070 Tool/software: Hello,
For SDI Serializer part LMH0070SQE/NOPB, there are following LVDS Input pins "TX[4:0]+", "TX[4:0]-" and "TXCLK+","TXCLK-"
Does these input pins support LVDS standard only or Differential 2.5-V SSTL Class…
Part Number: LMH0070
Tool/software:
Hi expert,
How much current does the VDDPLL pin consume? (We are preparing IR drop simulation and gathering the necessary information.)