Part Number: LMH0303 Other Parts Discussed in Thread: LMH0397 Dears
We are wondering if this part can work as end input and , dual single end output? like covert one signal end signal to two single end signal? thanks
B.R.
Jun Shen
Part Number: LMH0303 Hello,
I use the LMH0303 as the cable Driver for a 3G-SDI camera. But time to time and sporadically I get multi images as follow!
While the Eye-Diagram still looks good!
What could be the reason?
Part Number: LMH0303 Hi,
We are using LMH0303 cable driver, the ouput of the driver is going to a 75ohm HF connector(Attaching the schematic).
The Output voltage swing is around 768mV and 270ps to 320ps, but the eye diagram shows lot of distorted. We…
Part Number: LMH0303 Other Parts Discussed in Thread: LMH0397 Hi all,
we are using LMH0303 to convert 3G-SDI 100ohm differential signal to 75ohm single-ended output.
We have an issue with the output signal (bad eye diagram).
As first we had suspicions…
Part Number: LMH0303 Other Parts Discussed in Thread: LMH0302 , DS30BA101 Hi,
I plan to use the LMH0303 cable driver to drive a 50R cable rather than 75R. This is for a video application running at 2.97Gbps, but with a bespoke protocol (i.e. it's not 3G…
Part Number: LMH0303 Hi,
RSTI & ENABLE pin of LMH0303 has internal pull-up resister. Please let me know these resistance value including tolerance. Best regards, Akira Sakai
Part Number: LMH0303 Team,
ordering LMH0303SQ/NOPB from TI Store, does the device come with standard, max. 2y shelf life?
Asking since we see that ESL (5y) is also available for this device.
For one of our projects, it's crucial that the material is not…
Part Number: LMH0384 Other Parts Discussed in Thread: TINA-TI , LMH0303 , , LMH0397 Tool/software: TINA-TI or Spice Models Hi,
Is there any plan to release IBIS-AMI models for LMH0384 and/or LMH0303? I have these parts on a board and need to do some HyperLynx…
Part Number: LMH0303 Dear Sir/Madam,
I encountered SDI jitter issue with vertical transition jumping (see attached SDI_Jitter.mp4). LMH0303 is driven by Xilinx XC7A200T SDI IP, and SDI clock is driver by ASEMPLV-148.500MHz-LR-T.
Do you have any advice…