Part Number: LMH0318 Hallo All,
I'm using the LMH0318 driven by the FPGA.
The video reclocking feature is working.
I'm also configured the device in IRQ mode (on LOS pin) to monitor the status of the device.
I'm performing a test to validate the…
Part Number: LMH0318 Other Parts Discussed in Thread: LMH0324 Hello,
I am having issues with signal integrity with the LMH0318. I have a PCB with four identical circuits using these parts, however, when it comes to testing them I have found that some…
Part Number: LMH0318 Tool/software: Hello,
I have a question about select channel register command, if we send it, do the registers return to their default values?
Thanks,
Part Number: LMH0318 Other Parts Discussed in Thread: USB2ANY , LMH1218EVM , LMH1218 Tool/software: We have a LMH1218EVM where we removed the LM1218 and replaced it with a LMH0318. Jumpers configured for SMBus mode per the LMH1218 EVM User Guide. Running…
Part Number: LMH0318 Tool/software: Hello,
I'm using an LMH0318 to create an SDI selector and would like to know the video switching time between IN0 and IN1 both on OUT0.
Thanks,
Part Number: LMH0318 Tool/software: Hello,
There is a short circuit protection that can be enable via bit drv_1_sel_scp. Can you explain how it works? What will happen in case of a short circuit?
Is there a reason why this short circuit protection…
Part Number: LMH0318 Tool/software: Hi E2E team,
I am not finding the Input Mux switching time for the LMH0318, is it there any specification, or expected value, for this?
Thanks. Have a great day
Part Number: LMH0318 In my project iam using this lmh0318 IC it have two interfaces SPI,I2C.For SPI its voltage level is 2.5V,for I2C its 3.3V tolerant,The I2C interface should 3.3V? can we connect to 2.5V is operate correctly?
Part Number: LMH0318 Other Parts Discussed in Thread: LMH0340 , LMH0341 Can i give common clock,data I2C interface for the following devices
lmh0341,lmh0340,lmh0318.