Part Number: LMH0324 Other Parts Discussed in Thread: LMH0318 Hello,
I must isolate the SDI signal on the PCB board. So my idea was to use a balun at the input. It should transform the unbalanced Signal from the BNC connector to an balanced signal, which…
Part Number: LMH0324 Other Parts Discussed in Thread: LMH0318 , , LMH1218EVM , LMH1218 , LMH1219EVM , LMH1219 Hi Team,
We would like to ask your help regarding the customer's inquiry below.
I'm planning on developing a HD-SDI 2:1 switch using 2 x LMH0324…
Part Number: LMH0324 Other Parts Discussed in Thread: LMH1219 Hi Team, I see LMH0324 programming guide and have a question. The programming guide shows "IN1" in many places. I believe LMH0324 has one input (IN0 only) so how to consider "IN1"?…
Part Number: LMH0324 Other Parts Discussed in Thread: LMH0302 , LMH1219 , LMH1219EVM Tool/software: Code Composer Studio We have customer feedback that our SDI allocator scheme does not transmit as far as Semtech's scheme.Said that in the same use environment…
Greetings,
1)/ Suggestion is to first use LMH0324 or LMH0384 instead of LMH0387. This is because you just need an equalizer. LMH0387 has more functionality and it is not needed in this application.
2). You do not need LVDS to CML converter. Please AC…
Part Number: LMH0324 Dear Sir or Madam,
I would like to operate the LMH0324 without any programming. The operation I like to achieve is, that a 1,485 Gbps HD-SDI Signal is simply passing through the device, so that I can handle it on the 100 Ohm differential…
Part Number: LMH0324 Other Parts Discussed in Thread: LMH1219 I am designing a power supply for 8x LMH0324 and I am looking for the worst-case power consumption. We are using a 2.5V rail.
Per the data sheet, IDD is listed as 71 mA max at 2.5V (6.4 "Electrical…
Part Number: LMH0324 Other Parts Discussed in Thread: LMH0302 LMH0324 configuration parameters are as follows
0x00=0x08
0x27=0x04
0x30=0xA3
0x31=0x63
0x32=0x00
0x33=0x00
Greetings Shinichi-San,
1). I checked LMH0344 and we do not have CS pin. Could you please double check with the customer?
2). Also, LMH0344 is one of the older 3G SDI equalizer. The latest 3G SDI equalizer is LMH0324. Please note data sheet below. Please…
Hi Conor,
By expanding loop bw, you are passing all the jitter to the device attached at the output of the device(LMH0397) - for example FPGA or ASIC receiving signal from LMH device. In this case, you can just bypass CDR as you noted. Or you can also…