Part Number: LMH0324 Other Parts Discussed in Thread: LMH0397
Hi all,
I'm looking for a simple solution for an SDI-HD repeater with carrier-detect function.
The signal source is SDI-HD camera with BNC.
The output MUST be the same as the input signal…
Part Number: LMH0324 Hi
The spec'ed max rate of this part is 2970Mbps. Running a 3G SDI signal that puts the rate right at 2970Mbps without any head room. Is this going to be an issue? Sometimes the max rate of a standard interface is slightly higher…
Part Number: LMH0324 Other Parts Discussed in Thread: LMH1219 Hi
We would like to read the lock data rate.
Following LMH0324 programming P.11, 4.2 CTLE/CDR Register Page
Thus we follow LMH1219 procedure shown below. However register 0x02 bit [4:3] are…
Part Number: LMH0324 I'm looking for the full data sheet for the LMH0324 as well as any results for return loss performance.
I did see another thread discussing the data sheet, however I could not find the "Special Notes" section that was referred…
Hi Andrei,
Andrei Ziganshin said: Just would like to confirm that a single LMH0397 is capable of equilizing 2 separate inputs? Or do I connect the first two inputs (INPUT1, INPUT2) to LMH0397 which is configured as Cable Driver mode for switching first…
Part Number: LMH0324 Dear Support team,
Our customer will use LMH0324 in their application. Set IN_OUT_SEL = F to disable OUT1 and use only OUT0.
What should we do with the LMH0324 unused output pins ? (OUT1+, OUT1-) I believe you could leave output pins…
Other Parts Discussed in Thread: LMH0324 , LMH0318 Dear Technical Support Team,
I have a question about LMH0324-18EVM.
I can't find datasheet of LMH0324-18EVM. I'd like to see schematic of this board.
How can we get it? Is it based on NDA?
http…
Hi Nan,
LMH0394, LMH0324, or LMH0397. Would work for this application. Customer use any of these parts. Please note 100-ohm output requires AC coupling to the FPGA or ASIC.
Regards,Nasser