Part Number: DS25CP104A Other Parts Discussed in Thread: LMH0324 , LMH0318
Hello,
we want wo use the DS25CP104A switch in an 3G SDI application (multiplexer with 4 inputs / 4 outputs).
The new device/circuit must support following function:
It must be…
Part Number: LMH0318 Other Parts Discussed in Thread: LMH0324 , DS25CP104A , Hello,
we have developed a 3G-SDI switch with the following TI components:
Equalizer: LMH0324
Switch: DS25CP104A
Reclocker/Cable Drive: LMH0318
If I power on the device without any…
Part Number: LMH0318 Other Parts Discussed in Thread: LMH0397 , LMH0324 Hello,
Is there an existing linux kernel driver for LMH0318 device ?
Regards,
Bruno
Part Number: LMH0318 Other Parts Discussed in Thread: LMH0324 Hi,
I need to know the common mode voltage of the LMH0318 inputs. Can anybody helb me?
Please take also notice to my other thread, where I need to know the common mode voltage of the LMH0324…
Part Number: SN65LVCP408 Other Parts Discussed in Thread: LMH0324 , , LMH0318 Hello!
I am trying to design somewhat of a multiple SDI switcher. Starting with the LMH0324 Equalizer, going to the SN65LVCP408, and then being reclocked and driven with the LMH0318…
Part Number: TIDA-03028 Other Parts Discussed in Thread: LMH0318 , LMH0324 , MSP430F5529 , SIGCONARCHITECT , , USB2ANY Dear Forum,
I want do build a new PCB Cuircuit with two LMH0324 and one LMH0318.
My Question:
Can I use a new MSP430F5529 Controller to communicate…
Greetings,
At 3Gbps data rate, we should not connect outputs in parallel.
Suggestion is to use four LMH0324 or LMH0344 and then send outputs to DS25CP104 - 4X4 LVDS cross point. LMH0324 has better performance and lower power consumption than LMH0344.Also…
Part Number: TDP158 Other Parts Discussed in Thread: LMH1297 , LMH0324 Hi,
May I know TI have any Long rang image transfer solution? >100m is better.
Thanks!
Jeff
Hi Frank,
1). Input to the LMH0307 device is 100-ohm differential input or 50-ohm single ended. Device does not accept 75-ohm single ended input.
2). LMH0307 can output two 75-ohm single ended signals.
3). Please take a look LMH0324 device( https://www…
Hi Gaurav,
All of TI 3G SDI equalizers are adaptive. This is because in normal application cable length attached to the device is un-known. Therefor 3G SDI needs to be adaptive. For adaptive 3G SDI equalizer please consider LMH0324 device. Below is a…