Greetings,
Please below find parts with similar functionality and more:
1). GS2984: 3G SDI Equalizer LMH0384(pin compatible) and LMH0324(not pin compatible but superior performance and 12G SDI compatibility).
2). GS12241: 12G Equalizer with reclocker…
Hi Ali,
You should use an FPGA - after LMH0341 - to convert from SMPTE 292 frame format to CSI-2 frame format. Alternatively, you can also use a device linke LMH0324 and directly connect this to the transceiver input of the FPGA. Then FPGA would do…
Hi Lian,
While LMH0344 could work for this application, LMH0324 and LMH0397 devices have added advantages by offering longer cable reach and retiming functionality respectively. Please have your customer consider one of these three devices( LMH0344…
Hi Bang,
An example of a 3G-SDI Cable EQ is the LMH0324, which is a device that adaptively equalizes based on the length of cable you insert on the BNC connector. The Cable EQ provides frequency-dependent equalization to counteract the effect of attenuation…
The LMH0324 can equalize up to 280 meters of 75 ohm coaxial cable at 1.485 Gbps.
Similar devices are located at: www.ti.com/.../serial-digital-interface-products.page
Regards,
Lee
Hi Nir,
SD3GDAIII used our older generation of 3G devices.
Please instead use the following reference design collatorals:
http://www.ti.com/product/LMH0324/toolssoftware
This design uses LMH0324 and LMH0318 - our latest 3G equalizer and cable…
Hi Satoshi-san,
Sorry for the delay in response.
Yes, the LMH0324 is capable of compensating more than 4-5 dB attenuation loss, since the maximum Belden 1694A cable it can equalize is about 200m at 3G and 280m at 1.5G. Please enter a request for more…
Hi Raja,
For a 2:1 mux, I recommend trying a combination of 2 x LMH0324 cable EQs and 1 x LMH0318 cable driver.
- The LMH0324 is a newly released 3G-SDI equalizer and achieves better cable reach performance than the previous generation LMH0344.
…
Hi Martin,
Current consumption would be the same as long cable.
In later equalizers like LMH0384 and beyond(LMH0394 or LMH0324) we implemented auto sleep feature. In this mode, device completely powers down signal path and power consumption is minimum…