Part Number: LMH0340 Other Parts Discussed in Thread: LMH0341 Tool/software: Hi team,
We are doing simulation in Hyperlinks, we are not able to open the given simulation models for the below parts in the tool.
LMH0340 DS32ELX0421 IBIS Model .
LMH034…
Part Number: LMH0341 Other Parts Discussed in Thread: LMH0394 , LMH0344 , LMH0324 , LMH0340 In LMH0341(SDI TO LVDS) applications:
SDI Adaptive Cable Equalizer LMH0344/LMH0394,Which is suitable for LMH0341?
Part Number: LMH0341 Hello,
I have a question about the maximum current rating for the LMH0341. In the datasheet it specifies a maximum of 77 mA for the 2.5V supply in 3G with loop-through off, and a max of 120 mA on the 3.3V supply when loop-through…
Part Number: LMH0318 Other Parts Discussed in Thread: LMH0340 , LMH0341 Can i give common clock,data I2C interface for the following devices
lmh0341,lmh0340,lmh0318.
Part Number: LMH0341 Can LMH0341 transform SDI signal to output signal of LVDS type?
Thanks!
And if TI have some scheme transforming SDI signal to USB output signal?
And if TI have some scheme transforming SDI signal to PCI-E output signal?
And if TI have…
Part Number: LMH0341 hello
We are using LMH0341 and SD-SDI Video Protocol, we Connect LMH0341 LVDS output to FPGA Xilinx Spartan-6 XC6LSX9-2tqg144.
in VHDL Program ; we use 27 MHz Clock and when event rising edge and falling edge we get 5-bit data from LVDS…
Part Number: LMH0341 Hi team,
I cannot download LMH0341 code through http://www.ti.com/tool/broadcast_video_serdes_ip
Below is the error message.
Thanks,
Miranda
Part Number: LMH0341 Hi team,
The customer only uses 4 data output pins,but it has 5 data output pins for LMH0341.
He wants to get if he can use LMH0341 for his application. If he can, how to deal with the unused data output pin?