Part Number: LMH0341 Do you need to put AC caps between the LMG0341 and the FPGA video lines? The typical application circuit does not have anything and there's no mention of it.
Part Number: LMH0341 Hi team,
The customer is using LMH0341. He needs the Receive XILINX IP.
I found this link:
Is the Xilinx Spartan Example Code the customer's requirement in the link?
But I cannot download the code in the link. Would you send me…
Part Number: LMH0341 Other Parts Discussed in Thread: LMH0344 , DS90CF386 , DS90CF384 , SN75LVDS82 Hello,
I was hoping I could get some assistance with a design I'm working on. I'm looking for a way to take a 3G-SDI signal and convert it to an LVCMOS parallel…
Part Number: LMH0341 Other Parts Discussed in Thread: LMH0340 ,
Tool/software: Code Composer Studio
Hello,
I'm looking for
1) A Deserializer, which supports 3G-SDI as input and 16-bit BT.1120 as output.
2) A Serializer, which supports 16-bit BT.1120 as…
Hi Adrien,
Since we have not characterized/tested the device in this configuration - DDR/2 - we cannot guarantee this operation. We should closely follow figure 3 of the data sheet timing.
One thought crossed my mind, can you control TX clock ppm tolerance…
Part Number: LMH0341 My task is to deserialize the DVB-ASI stream and to transport the MPEG-TS data over ethernet.using the UDP protocol. I do have a Spartan 3E Fpga board but i never use FPGA's before and i think that it will be a very hard task for me…
Part Number: LMH0341 Hi Team,
Will output of LMH0341 be compatible with MC20902? MCP20902 is an FPGA bridge to convert LVDS to MIPI D-PHY.
Regards,
Mahendra
Hi Amy,
1). Complete 10 bits need to be provided to the LMH0030 device. 10-bits X 27MHz is equivalent to 270MBps.
2). 10 Bits at 27MHz clock can be used to meet these two requirements.
3). Typically FPGA along with a serializer is used. There are two…
Other Parts Discussed in Thread: LMH0340 , LMH0341 , DS32ELX0421 , DS32ELX0124 Dear Technical Support Team,
Do you have simulation models like IBIS mode and SPICE model for LMH0340 and LMH0341?
Best Regards,
ttd