Nasser,
In the battle of power dissipation I don't think I have enough margin for the LMH0346.. the LMH0366 appears to be my direction of design travel.. This being said.. I've not found any further details from Jay's posting with respect to the 4.7pF…
Hi Dave,
I haven't seen any customer issue related to the EMI(as long as LMH0366 is concerned). However, LMH0366 is sensitive to adjacent VCO or similar frequency. My suggestion is if you are happy with LMH0346 then perhaps it would be a good idea to…
Other Parts Discussed in Thread: LMH0303 , LMH0384 , LMH0366 Hi Expert
Our customer Eoptolink is debugging LMH0366, LMH0303, LMH0384. They reported issue of LMH0366.
Issue descriotion: When testing with SMPTE pattern (270M, 1.485G, 2.97G), with CDR…
Last year, I've received a Jitter transfer VS CP current plot with 0.2UI input jitter.
Well, Other customer want to see a same plot with 3UI input jitter.
Do you have a jitter transfer data with 3UI input jitter ?
Please let me know a delay time from a valid singnal in to Register address 0x03 bit:4 = 1 ? Also from a Vailod signal stop to Register address 0x03 bit:4 = 0 ?
We have a customer who wants to use "SD3GDAIII kit." "SD3GDAIII" User’s Guide (snlu112.pdf) section 3.5 in displayed about the eye patterns. I ask the following questions.
(1)Is there any waveform for comparing Oscilloscope waveform? (2)Are there any…
Other Parts Discussed in Thread: LMH0366 , LMH0346 I have samples of the LMH0366 3G-SDI re-clocker IC but no data sheet. I can't finish the design without the pin-out. The online data sheet does not have pin-out information. If the samples exits, then…
Other Parts Discussed in Thread: LMH0376 , LMH0366 Do you have a Schematics and board Layput for LMH0366 ?
I know we can refer to the 3GDAIII manual and LMH0376 Sche and Layout.
But my customer want to see a recommendation Layout for LMH0366(24pin…
Hi all,
The MADI characteristic of LMH0366 (one input) 1) eye-patterns monitor. Although I had capture of 3G-SDI photographed last time Can you capture in AES-10 (MADI) 125MBit/sec?
2) Gitta zone At LMH0356 , it is SPI communication. Jitter Transfer…