Part Number: LMH1226 Hello
I'd like to know under which circumstances the OUT0/1 differential outputs of LMH1226 can be DC connected to its destination, without bulky series capacitors.
I don't see any statement in the datasheet concerning the common…
Part Number: LMH1226 Hi Team,
Our customer would like to know if the LMH1226 can be connected directly to a SFP video optical transceiver directly.
Regards,
Danilo
Part Number: LMH1226 Other Parts Discussed in Thread: LMH1219 Hi All,
Could you please provide the IBIS model of LMH1226? There was an IBIS model request from a customer.
Best Regards, Ishiwata
Part Number: LMH1208 Other Parts Discussed in Thread: LMH1297 , LMH1226 , LMH1219 , LMH1218 , LMH1228 , LMH1297EVM , LMH1229 Tool/software: We are being asked to design a 3U 160 mm card with e 75-ohm BNC to 100-differential convertor. The signal speed is 3G…
Part Number: LMH1226 Other Parts Discussed in Thread: LMH1297 Are there any registers to lower the loop bandwidth on the LMH1226 for 12G rates?
Thanks
Jason Hartle.
Part Number: LMH1219 Other Parts Discussed in Thread: LMH1226 , Hi team,
In TI_LMH1219_LMH1226_IBIS_AMI_User_Guide.pdf , S port sequence is 1->2, 3->4. but in tx_term0-7.s4p, S port sequence is 1->3, 2->4. which is correct?
Thanks!
Rayna
Part Number: LMH1226 I have few questions about LMH1226 as following.
1) Is there a NVM inside to store register setting or it needs a external MCU?
2) If I select CTLE/CDR register page or drivers register page, how can I go back to share register page…
Part Number: LMH1226 Other Parts Discussed in Thread: LMH1219 ,
I think board design is almost the same between LMH1226 and LMH1219.
LMH1219 EVM has 9 vias on thermal PAD land. However the vias number are 5 in "Layout Example" and "Example Board Layout…
Part Number: LMH1226 Other Parts Discussed in Thread: LMH1219 , LMH1218 Hi Team,
I see below NOTE in the LMH1226 datasheet. Could you please help us understand the CDR Reset and Release requirement ?
Q1). I understood that LMH1226 will start CTLE adaptation…
Part Number: LMH1226 I've heard that it is recommended to add additional 0.01uF capacitor to each power pin (VIN, VDDIO, VDD_LDO and VDD_CDR) of the datasheet Fig 27 configuration.
Is this needed for all power pins?
Our customer has space limitation…