The inductor is the "MPL-AL5030-4R7" from Monolithic Power Systems
C32: 25V
C48: 25V
C50: 10V
C51: 25V
C22: 10V
VIN: Should be approximately 13VDC to 16VDC.
IOUT: Up to 500mA, but typically 100 to 200 mA
Bottom:
Inner Layer 1 (IL1…
Part Number: TPS5410-Q1 Other Parts Discussed in Thread: LMR66410-Q1 Hi,
In the app note SLVA237C , the compensation loop is modified in case ceramic capacitors (very low ESR) are used. My question is: In case the inductor already provides high ESR…