Part Number: LMS3655-Q1 Other Parts Discussed in Thread: LM73606-Q1 , LM73605-Q1 Tool/software: WEBENCH® Design Tools Hi Team, My customer considers to use LMS3655-Q1 for the following automotive application. ---------------------- Vin: 18 - 36V *ABS MAX…
Part Number: LM60430 Other Parts Discussed in Thread: LMS3655-Q1 , , LMS3655 Hello,
I would like to ask you a question about the LM60430A. When calculating the efficiency with WEBENCH, it is 97.55% as shown in the attached result. For reference, the LMS3655…
Other Parts Discussed in Thread: LMS3655 , LM61460 , UCC28781 We have Vin 22-32V and Vout 20V 100mA.
Currently we are using LMS3655 in a flybuck mode.
I dont understand why there is LM61460 as a suggestion and described as "lower EMI" when the datasheet shows…
Part Number: LMR23630 Other Parts Discussed in Thread: LMS3655 Hello,
I want to know how I get the switching quiescent current(no load input current) value of LMR23630
Some datasheet such as LMS3655, it's shown how to calculate the switching quiescent…
Part Number: TPS62913 Other Parts Discussed in Thread: LM61440 , LMS3655 , LMR33640 , TPS55288 , TPS56637 , LM61460 The (3 to 17V input, 3A output) TPS62913 is a very interesting Vreg IC. In addition to combining the PSRR of an LDO and the efficiency of a…
Hi Martin,
we don't have pin2pin or similar package part. The few available options are: TPS565208, TPS56637, LM73606, LMS3655. Please check the datasheet to see whether they are fine. If not, you can add more output capacitor to TPS56628.
Jmmn,
Reply as below,
1,Can you confirm if USB_VBUS to the hub toggles low when the hub is not connected to the host controller?
-- The same U disk is sometimes detected and sometimes not detected,the test Vbus waveform as below,no dropdown.
2,What kind…
Part Number: LMR23625-Q1 Other Parts Discussed in Thread: LMS3655-Q1 , LMS3655 , LMR23625
Dear Team,
similar request like my previous post about the LMS3655-Q1 , but the customer has new specs (lower output currents):
V-in = car battery
V-out = 5V
I-load…