Part Number: TPS3870-Q1 Hi Team,
Our customer needs to control the opening of an N - Channel MOSFET via the RESET pin and would like to understand whether this is possible by connec ting the RESET pin to a voltage sou rce via a pull-up resistor?
I…
Part Number: DS90UB935-Q1 Hello Team,
I got a question from customer.
They plan to perform spread spectrum for CSI_CLKP/N signal by their CSI-2 clock source.
The spread range is not decided yet but they assume it will be ±2.5% or ±5%. Can you please…
Part Number: TLV320AIC3104-Q1 Hi TI team,
Please provide SNR in dB (A-weighted) and THD+N in % @1KHz as shown in the image below
1. TLV320AIC3104-Q1 is connected with TPA3118D2QDAPRQ1 and gain set to 9Kohm
Part Number: DS90UB948-Q1 Hi team
what's the CMLOUTP/N range of 948 and 928? in the datasheet, only show the typical value is 360mV. what's the maximum and minimum ?
thank you
Part Number: LM5150-Q1 Hello Team,
My customer asked if the N-channel MOSFET of LM5150-Q1 can be changed from NVMFS5C466NLT1G to IPZ40N04S5L-7R4 or IPZ40N04S5L-7R4 due to limited PCB space. So please review and coment if the IPZ40N04S5L-7R4 and IPZ40N04S5L…
Part Number: LM4041-N-Q1 Other Parts Discussed in Thread: REF34-Q1 , REF31-Q1 , REF2025 , INA240
Dear team,
My customer uses our LM4041AIM3-1.2/NOPB, and the temp range is -40-85C. Based on testing, they found that the temp range is too small, and…
Part Number: LM4050-N-Q1 Dear team,
For this device, there is no output capacitor required. If the customer wants to add capacitors to reduce noise, is there a maximum capacitor limit?
Thanks & Best Regards,
Sherry
Part Number: DS90UH948-Q1 Other Parts Discussed in Thread: ALP Hi Team,
FPD-link has the bi-directional control channel.
From Ser to De-Ser is the forward channel.
From De-Ser to Ser is the back channel.
Is it possible to turn off the back channel…
Part Number: UCC27284-Q1 Other Parts Discussed in Thread: UCC27284 Dear TI Team,
this is regarding an application circuit of : Half-Bridge Gate Driver to Drive a High Side Back-to-Back N-MOSFETs (in Common-Source Configuration)
When we disabled HI…
Part Number: DP83TC811S-Q1 Hi team
I would like to ask that if our DP83TC811SQ1 could support function like this:
That is to say, the requirement is whether the P and N of the external connector are connected positively and negatively(inversely…