Part Number: LP-CC2652RSIP Other Parts Discussed in Thread: SIMPLELINK-CC13X2-26X2-SDK Hi Sir,
I encountered a problem. There are two open declaration. How do I choose the position I want?
BR,
Amos
Part Number: LP-CC2652RSIP Other Parts Discussed in Thread: CC2652RSIP , SYSCONFIG When I attempt to build a RTSC project (For example, the project /Applications/ti/simplelink_cc13xx_cc26xx_sdk_5_30_01_01/examples/rtos/LP_CC2652RSIP/ble5stack/simple_mesh_node_oad_offchip…
Part Number: LP-CC2652RSIP Other Parts Discussed in Thread: UNIFLASH , CC2652RSIP I have encountered problems when changing a random static address using the HCI_LE_SetRandomAddressCmd. I am using simplelink_cc13x2_26x2_sdk_5_20_00_52. The first problem…
Hi Ryan,
zr_sw_ota_client_offchip example works in both LP-CC2652RSIP and custom board which I tested successfully. when ever I checked with the zr_genericapp example, OTA process starts successfully stuck at some percentage 60%. that means not getting…
Part Number: CC2652PSIP Other Parts Discussed in Thread: , LP-CC2652RSIP , UNIFLASH , CC2652R7
Hello TI Team,
I’m currently working with the CC2652PSIP Development Kit and attempting to perform RF testing using SmartRF Studio 7 . As shown in the attached…
Part Number: UNIFLASH Other Parts Discussed in Thread: CC2652PSIP , CC2652RSIP , LP-CC2652RSIP Tool/software: Would like to program my CC2652PSIP device with lower TCLK rate, about 1MHz. With CCS it works correctly, I can debug my application. UniFlash…
Hi Kumaravel,
As we discussed in your previous E2E thread , you will need to ignore the existing Display TI Driver and focus solely on creating a new interface from the SPI TI Driver using the available examples . The SPI Pinmux will determine which…
Part Number: CC2652RSIP Hi Ti Team,
I tried to configure DIO31 as input, using the example project simple_peripheral with LP-CC2652RSIP.
it seem the PINCC26XX.c does not allow such configuration and the PIN_init() Failes.
we are using the CC2652RSIP…
Part Number: CC2652RSIP Dear Team,
I have LP-CC2652RSIP demo board.
It have not any matching circuit for antenna, there is only one capacitance I think it is for DC blocking.
In SYSCFG file front end mode: differential, Bias confugiration: Internal…