Part Number: LP-EM-CC2745R10-Q1 Other Parts Discussed in Thread: LP-EM-CC2755P10 Tool/software: The data sheet for CC2755x10 references the LP-EM-CC2755P10. When will this board be available?
Part Number: LP-EM-CC2340R5 Other Parts Discussed in Thread: LP-XDS110 , CC2340R5 Besides
LP-EM-CC2340R5
Will we need extra Hardware to connect the LP-EM-CC2340R5 to my USB PC?
If yes, please let me know what else will be needed
Thanks
Part Number: LP-EM-CC35X1 Other Parts Discussed in Thread: LP-XDS110ET Hello,
I am evaluating the LP-EM-CC35X1 LaunchPad using an LP-XDS110ET external debugger.
Development Environment
Code Composer Studio: 21.0.0
SimpleLink Wi-Fi SDK: 10.10…
Hi Sir,
I am using an LP-XDS110ET debugger to flash/debug the CC3551E device on our custom Renu board.
For the debugger connection, I have connected only the following four signals between the LP-XDS110ET and the CC3551E Target board:
GND
RESET…
Hi Sheng,
If the error still persists, please verify your activation type in sysconfig. It should match the type that you flashed with the device with:
Please let me know if this resolves the error.
Best Regards,
Josh Prushing
Part Number: LP-EM-CC2340R5 Other Parts Discussed in Thread: CC2340R5 , UNIFLASH Hi I am checking LP-EM-CC2340R5 EVK with Linux system. EVK is connected with Linux system using XDS110 debugger. I have flashed the EVK with host_test_LP_EM_CC2340R5_freertos_ticlang…
Part Number: LP-EM-CC2745R10-Q1 Other Parts Discussed in Thread: CC2745R10-Q1 Hi:
In studying the CAN communication function of the LP-EM-CC2745R10-Q1 development kit, do I need an additional CAN transceiver kit to test CAN communication? And what is…
Part Number: LP-EM-CC35X1 Tool/software: We have successfully imported and built the "simplelink_wifi_sdk_9_20_00_06_eng\examples\rtos\LP_EM_CC35X1\demos\network_terminal" project using CCS. However, we are encountering issues during debugging. Despite…
Part Number: LP-EM-CC2745R10-Q1 Other Parts Discussed in Thread: CC2745R10-Q1 We are currently attempting distance measurement between a Pixel 10 and a CC2745R10-Q1 LaunchPad. During the CS procedure, we are encountering a failure and would like to request…
Part Number: LP-EM-CC1354P10 Other Parts Discussed in Thread: BOOSTXL-SHARP128 I'm currently using (4 ea.) LP-EM-CC1354P10-1 for a project. One LP-EM-CC1354P10-1 is the Collector and the other three are used as the Sensor. I'm using both Collector_SM…