Part Number: LP2981A Tool/software: We are trying to confirm lot traceability information for our order of
LP2981AIM5-5.0 components. The documentation says 2106 and the markings on the part have the following:
Top: L03A
Bottom: 12H
Can you…
Part Number: LP2981A Tool/software: We have one of your components, a LP2981AIM5-5.0 that has been re-coated to a pure-tin finish. Our application requires that all of our components have tin-lead finish. Could this re-application of solder induce damage…
Part Number: LP2981A Other Parts Discussed in Thread: SN6501 , Hello TI team,
I need to implement an isolated CAN Bus node based on the spec sheet recommended design of the transformer driver SN6501.
Question 1
I would like to use the LP2981A…
Hello Nick,
The GND Pin was around 1V5
Looking at the LP2980 ADJ, it looks like, the internal band gap is a possible reason why the trick is not working.
There is something that goes wrong when GND is something else (Sink/Source current ???…
Part Number: LP2981A
HI:
https://e2e.ti.com/support/power-management-group/power-management/f/power-management-forum/998768/lp2981-to-know-the-concern-of-connect-the-lp2891-pin4-nc-to-ground/3694604
The LDO LP2981A-50DBVR of TI and pin 4 are NC…
Part Number: LP2981A Hi,
customer need to know.
1. if LP2981A-33DBVR has OTP (over temperature protection) function? if yes, what's the min, typ, max value?
2. what's the Vo accuracy of LP2981A-33DBVR at temperature range 125C to 150C?
thanks…
Part Number: SN65HVD1782 Other Parts Discussed in Thread: DRV5055 1.TPS70950DBVR The output current does not meet the requirement:50mA ≤ l ≤ 100mA.Can LP2981A-50DBVR meet the requirements?
2.SN65HVD1782 The pin sequence is not satisfied.Does TCAN1044AVDRQ1…
Hi McKyla,
I would still like to have an answer to the following question.
Are the following two part numbers effectively the same chip material?
LP2981AIM5-5.0 (from the LP2981-N datasheet)
&
LP2981A-50DBVR (From the LP2981 datasheet)
…
Thanks Jeff,
LP2981A is a fixed output voltage regulator, but I need an adjustable voltage regulator.
It would be very helpful for me if you could suggest any adjustable LDO regulator from TI., that is compatible with LMG1020.
Thanks
Hitesh K…