Part Number: LP5036 Other Parts Discussed in Thread: TLC59116 Hello team,
I'd like to confirm the use case for LP503x.
Is it possible to bund 3ch for 1 LED?
The reason why I'm asking this since the customer wants a higher current limit.
Their…
Part Number: LP5036 Other Parts Discussed in Thread: LP5030 Hello,
My questions are in regards to the chip enable (pin 43) of the LP5030/6.
When disabled via pin 43, does the I2C bus still work?
When disabled via pin 43, is the firmware still running…
Part Number: LP5036 Hi e2e Team,
I want to use two LEDs in a row connected to one OUTx pin on the LP5036. Is it possible to higher the VLED up to 9-12 volts if staying below the Output Maximum Voltage of 6V?
Thanks! Regards
Claudius
Part Number: LP5036 Hi Support team
my customer would like to use LP5036 to control more than 36 channel LEDs, as above reason, they need to adopt more than one LP5036, like 3 or 4 ICs,
however, may i know how many device could be controlled in one I2C…
Part Number: LP5036 Dear Team,
LP5036 according to datasheet requires a minimal time of the falling edge of SCL and SDA of 15ns -> after some research the finding was that mmight only be valid for frequencies > 100Khz (fast-mode). Customers only…
Part Number: LM5036 Other Parts Discussed in Thread: LP5036 Dear team,
Do we have LP5036 LED driver/code for Android/Linux ?
If yes, could you provide the LP5036 LED driver/code for Android/Linux to us?
Many Thanks
Jimmy
Part Number: LP5036 Other Parts Discussed in Thread: LP5012 , LP5569 Hi all,
I'm researching RGB LED low power drivers to a product. I recently found the family of the LP5xxx, and took a look in some options such as LP503x, LP5012, LP5569... they are…
Yes. The orange color is tricky - but yellow is basically impossible to achieve.
For orange - red-255, Green-40, Blue-0
I also learned that if I use the USCI_B_I2C_masterSendMultiByte... WithTimeout functions - I must check the returned value to determine…
Part Number: LP5036 Hello,
I'm looking at the following lines in the datasheet EC table:
Given two devices in a system, what is the maximum current error I could see between any two LEDs? Is it possible for two channels on separate devices to…