Hi Austin,
I think LP5861(T) could be a suitable option. Please contact me by email (jared-zhou@ti.com) if there are more detail requirements.
BR, Jared
Hi Muhammad ,
LP5861 is an 18 channel LED driver with 8-bit analog dimming and maximum current is 50mA which may suitable for your application.
https://www.ti.com/lit/ds/symlink/lp5861.pdf?ts=1683800059937&ref_url=https%253A%252F%252Fwww.ti.com%252Fproduct…
Part Number: TLC59116 Other Parts Discussed in Thread: LP5861 , LP5018
Hi Expert,
Can the TLC59116 adjust the color temperature? If yes, How to set it?
Hi Shinichi,
Considering this device is quite old material, so we cannot find the information you need.
But I'd like to recommend you our new device LP5861/LP5018, which are 18 channels LED drivers.
Thanks!
Part Number: LP5024 Other Parts Discussed in Thread: LP5861 Hi team,
Is the OUTx pins of LP5024 only supporting 5.5V abs max? Are there no OVP, right?
Regards,
Hayashi
Hi,
The frequency is calculated by below:
F = 160/(PSC + 1),so 100Hz cannot be achieved.
And if you set PSC0 = 0 and map the LEDs you want to use dim0,the frequency for these LEDs should be 160Hz.
If you want to achieve higher dimming frequency,you can…
Part Number: LP5018 Other Parts Discussed in Thread: LP5861 Hello,
I see this device has current limiting, but is there any kind of short circuit prtection? Or will the device be damaged in case of a short?
Thanks,
Michael
Hi Marc,
Considering the LP5018 only support 12 bits PWM dimming,so if you don't want to use PWM function,the device may not suitable for you,and series resistor cannot solve this problem because the current sink inside LP5018 will output a constant current…
Part Number: LP55231 Other Parts Discussed in Thread: LP5813 , LP5861 , LP5018 Hello,
I am using two LP55231 to control 6 RGB LEDs.
When I turn on all LEDs with max brightness, both ICs heat up to more than 80 degrees celsius. I stopped the testing as…
Part Number: LP5862 Other Parts Discussed in Thread: LP5861 Assuming we would like to use the LP5862 to only drive up to 16 LEDs and not in the 2x matrix arrangement, is it possible to connect the LEDs anodes directly to VLED instead of SW0, bypassing…