Part Number: LSF0102-Q1 Other Parts Discussed in Thread: TXS0102-Q1 Hi team,
I have a few questions regarding the LSF0102-Q1 devices.
I am planning to use these devices for I2C signals. In the datasheet, it is mentioned that the LSF0102-Q1 supports…
Part Number: LSF0102-Q1 Other Parts Discussed in Thread: TXU0202 Hello TI Team,
I am currently using the LSF0102-Q1 as a level shifter for UART communication between a 5V microcontroller and a 3.3V TI BLE wireless MCU (CC2745), as shown in the attached…
Part Number: LSF0102-Q1 Hi,
Is there an equivalent part to the LSF0102-Q1 in TI space enhanced plastic product line? looking for a voltage translator for MDIO bus (open drain) from 1.5 to 3.3V.
Or do you have radiation report for this device that…
Part Number: LSF0102-Q1 Hi,
I see published on the website that the device above has an MSL: 2 rating.
My receiving says they have material with an OEM label stating the MSL=1.
Is that possible?
Part Number: LSF0102-Q1 Other Parts Discussed in Thread: LSF0102 In a typical circuit design with LSF0102 shown as below.
If VCCB is powered by 3.3V, but Vref_A keeps 0V.
Is there leakage voltage from VCCB to Vref_A?
If there is leakge voltage,…
Part Number: LSF0102-Q1 Hi There,
For below mentioned configuration of LSF0102-Q1, IC is consuming ~25uA current during sleep mode. During sleep mode:
3.3V_BLE = 0V, 5V_MCU = 5V will be available.
B1 & B2 are pulled up with 1k.
I need to put…
Part Number: LSF0102-Q1 FIG 1
FIG 2
i am using LSF0102QDCURQ1 this part but i am confuse for the EN and Vref_B configuration .could you suggest which configuration is correct FIG 1 / FIG 2 with explination
Part Number: LSF0102-Q1 Other Parts Discussed in Thread: LSF0102 Hello TI,
We are developing communication device that has ethernet interface using data converting from 1.8V to 3.3V between ethernet phys, Now we are applying your chip LSF0102, however…