Part Number: MAX232E Other Parts Discussed in Thread: MAX3232E , TIGER Hi,
May I know the difference between MAX232E and MAX3232E?
Could they be replacement for each other?
Thanks and Best regards,
Tiger
Part Number: MAX232 Tool/software: Hi,
I have a few questions about MAX232IDR. Question: The current data rate of this material is 120Kbps. When using Baud rates 115200, the error of each bit delay is too large when RX is transmitted back to UART IC…
Part Number: MAX232E Tool/software: HI team,
Customer ask a situation when VS+ /VS- are not recoomended condition by accident.
Q1: When VS+ or V2- are open, what does it happens?
Q2: When a GND which VS+ / VS- connected thru 1uF become floating…
Part Number: MAX232 Tool/software: Hi Team
customer found the output peak voltage levels of pre-PCN and post-PCN device are different. is it normal? wht this happen?
Part Number: MAX232E Other Parts Discussed in Thread: ESDS552 , ESD652 Tool/software: I'm searching for a practical design guide especially for robust isolated interface, power distribution and grounding/shielding/chassis mounting within an embedded system…
Part Number: MAX232 Tool/software: We need UL Recognized Component (UR) certificates for below part.
MAX232DR
SN74LVC138APWR
SN74HC20DR
SN74LVC1G08DCKR
LM2596R-5.0V
LM2623Amm/NoPB
TPS61169DCKR
TPS54331DR…
Part Number: MAX232E Tool/software: Hi, I would like you to confirm about below. Q1, I understand that this device support up to 250kbps as data rate. So, I understand that this device support baudrate "115200 bps". Is my understanding correct ? Best…
Hello Ethan and Clemens, I understood that required rising time condition is different between MAX232E and application note example. In fact, case of MAX232E is "2us". On the other hands, if this device will meet 4% of unit interval, it should be "1.6us…
Part Number: MAX232 Other Parts Discussed in Thread: TCA5405 , SN74LV8153 , TSU6111A , TCAL9539-Q1 Hey Interface team,
I have a customer working on a project and we were hoping to get your advice on possible solutions to a design challenge we are running…
Part Number: MAX232 Hi there evrybody, I have recently ordered few MAX232N for a custom board whose function is to converter from RS232 to RS485 communication standard. While testing the behavior of the board, we encountered some complications. In order…