Part Number: MAX232 Hi team,
In customer's sysytem, SN75188NSRG4 has been used, but c ustomer is considering to repalce SN75188NSRG4 with MAX232NS in next project. Are there any concerns they need to take care about?
+/-12V is applied to SN75188NSRG4…
Part Number: MAX232E Other Parts Discussed in Thread: TRS208 , MAX208 Hi.
Please see the attached file.
I want to connect PCB1 DOUT1 and PCB2 DOUT1.
Is it possible?
If it isn't possible, do you have any ideas?
Besr regards.
MAX232E_question.xlsx
Part Number: MAX232 Dear specialists,
My customer is considering MAX232IDR and has a question.
I would be grateful if you could advise.
---
What is the maximum rating of the sink current of the driver / receiver OUT terminal?
I looked at the data sheet…
Part Number: MAX232 Hi
I am using 10uF Al El Cap with ESR and Ripple rate of 10 ohm and 60mArms. Now I need to change to 16ohms & 75mArms ripple current.
Will it cause any data rate malfunction because of change in Ripple current and ESR.
Part Number: MAX232 Other Parts Discussed in Thread: SN74LVC2G04 Hi team,
My customer is going to connect T1OUT to T2IN and R1OUT to R2IN to invert the signal.
Could you check it will not cause the damage of device?
Regards,
Saito
Part Number: MAX232 Other Parts Discussed in Thread: LM324 , Dear Team,
Do we have solution is that integrates function of MAX232 and LM324 ?
Many Thanks,
Jimmy
Part Number: MAX232 Hi team,
Could you tell the data rate when C1 = C2 = 0.085uF?
They need 12kbps at max but C1 and C2 are 0.085uF. So they are not sure this is OK, because C1 and C2 are 1uF at the condition of the datasheet. Could you give any suggestion…
Part Number: MAX232E since there is a typo in the datasheet for C1 to C4 (1mF in the Datasheet instead of 1µ real) I would like to know if the same error also happend with CBypass.
Part Number: MAX232E Other Parts Discussed in Thread: MAX208 , TRS208 Hi there,
I am working with the Medical SEM team to provide some alternative solutions for a customer that is redesigning their surgery system.
Is this device an adequate replacement…